Skip to main content
piernov
Associate
April 2, 2021
Question

X-CUBE-AI 6.0.0 (Windows): ImportError: cannot import name 'get_all_providers' from 'onnxruntime.capi._pybind_state'

With a fresh installation of STM32CubeIDE 1.6.1 on a clean WIndows 10 Pro 20H2, after adding X-CUBE-AI 6.0.0 to a new STM32 project, Analyze fails with:

ImportError: cannot import name 'get_all_providers' from 'onnxruntime.capi._pybind_state' (C:\Users\Utilisateur\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Utilities\windows\onnxruntime\capi\_pybind_state.pyc)

On ArchLinux (not a clean installation), the error does not seem to occur.

How to reproduce:

Create a new STM32 project.

In the board selector choose (for example) Nucleo-L452RE-P, validate project creation.

Add the X-CUBE-AI 6.0.0 software pack to the project with the Validation application template.

Create a new network and import your model (Keras used here).

Try to Analyze

Actual behaviour:

Analyze fails with:

Analyzing model 
C:/Users/Utilisateur/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/6.0.0/Utilities/windows/stm32ai analyze --name network -m C:/Users/Utilisateur/Documents/d1-notebooks/mnist_lenet5.h5 --type keras --compression 1 --verbosity 1 --workspace C:\Users\UTILIS~1\AppData\Local\Temp\mxAI_workspace16985705420013710289337304763638 --output C:\Users\Utilisateur\.stm32cubemx  
[4392] Failed to execute script stm32ai 
C:\Users\Utilisateur\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Utilities\windows\onnxruntime\capi\_pybind_state.py:14: UserWarning: Cannot load onnxruntime.capi. Error: 'DLL load failed: The specified module could not be found.'. 
Traceback (most recent call last): 
  File "stm32ai.py", line 959, in <module> 
  File "c:\python37\lib\site-packages\PyInstaller\loader\pyimod03_importers.py", line 493, in exec_module 
  File "onnxruntime\__init__.py", line 13, in <module> 
ImportError: cannot import name 'get_all_providers' from 'onnxruntime.capi._pybind_state' (C:\Users\Utilisateur\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Utilities\windows\onnxruntime\capi\_pybind_state.pyc)

Expected behaviour:

Analyze proceeds without error.

Temporary workaround:

Downgrade to X-CUBE-AI 5.2.0. With this version, Analyze completes successfully.

This topic has been closed for replies.

1 reply

piernov
piernovAuthor
Associate
April 19, 2021