Skip to main content
MYChen
Associate II
September 13, 2021
Question

What the mean of "list index out of range"and 'params set for InstanceNormalization layer'?This is my first time to use cubemx,so I'm confused.Could anyone help me?Thanks!

When I use cubemx.ai to analyze a onnx model ,I get a error tells list index out of range,what should I do? When I analyze another onnx model ,it occur another error 'params set for InstanceNormalization layer'Could anyone help me?Thanks:confounded_face:

    This topic has been closed for replies.

    6 replies

    MYChen
    MYChenAuthor
    Associate II
    September 13, 2021

    The model I use is a model which is transformed form pytorch to onnx.The model has no problem in pytorch and onnx.

    MYChen
    MYChenAuthor
    Associate II
    September 13, 2021

    error1:params set for InstanceNormalization layer0693W00000Dmwb3QAB.pngerror2:list index out of range0693W00000DmvrKQAR.png 

    MYChen
    MYChenAuthor
    Associate II
    September 13, 2021

    The error about wish can be fixed by 'sudo apt-get install tk'.However I don't know why it will occur error 'list out of range'

    fauvarque.daniel
    ST Employee
    September 13, 2021

    Can you share the model reproducing the error (or a dummy untrained one)

    Thanks

    Daniel

    ​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    MYChen
    MYChenAuthor
    Associate II
    September 14, 2021

    Thank you for your kindness. I'll write these down below.

    These models use pytorch:

    1.

    class Encoder(nn.Module):

    def __init__(self,input_nc=1,ngf=64,C_channel=4, n_downsampling=3,norm_layer=nn.InstanceNorm2d,max_ngf=256, Conv_type="DW"):

    assert(n_downsampling>=0)

    super(Encoder, self).__init__()

    activation = nn.ReLU(True)

    model = [nn.ReflectionPad2d(3), my_Conv(input_nc, ngf, kernel_size=7, padding=0, Conv_type=Conv_type, norm_layer=norm_layer, activation=activation), norm_layer(ngf), activation]

    ##downsample

    for i in range(n_downsampling):

    mult = 2**i

    model += [my_Conv(min(ngf * mult,max_ngf), min(ngf * mult * 2,max_ngf), kernel_size=3, stride=2, padding=1, Conv_type=Conv_type, norm_layer=norm_layer, activation=activation),

    norm_layer(min(ngf * mult * 2, max_ngf)), activation]

    self.model = nn.Sequential(*model)

    self.projection = nn.Sequential(*[my_Conv(min(ngf*(2**n_downsampling),max_ngf),C_channel,kernel_size=3,stride=1,padding=1, Conv_type=Conv_type, norm_layer=norm_layer, activation=activation),norm_layer(C_channel),nn.Sigmoid()])

    def forward(self, input):

    z = self.model(input)

    return self.projection(z)

    ​

    2.

    class Decoder(nn.Module):

    def __init__(self,ngf=64,C_channel=4, n_downsampling=3,output_nc=1,n_blocks=3, norm_layer=nn.InstanceNorm2d,padding_type="reflect",max_ngf=256, Conv_type="DW", Dw_Index=None):

    assert (n_blocks>=0)

    super(Decoder, self).__init__()

    activation = nn.ReLU(True)

    mult = 2 ** n_downsampling

    ngf_dim = min(ngf * mult, max_ngf)

    model = [my_Conv(C_channel,ngf_dim,kernel_size=3,stride=1,padding=1, Conv_type=Conv_type, activation=activation, norm_layer=norm_layer),norm_layer(ngf_dim),activation]

    ​

    for i in range(n_blocks):

    model += [ResnetBlock(ngf_dim, padding_type=padding_type, activation=activation, norm_layer=norm_layer, Conv_type=Conv_type)]

    ​

    for i in range(n_downsampling):

    mult = 2 ** (n_downsampling - i)

    model += [my_Deconv(min(ngf * mult,max_ngf), min(ngf * mult //2, max_ngf), Conv_type=Conv_type, norm_layer=norm_layer, activation=activation),

    norm_layer(min(ngf * mult //2,max_ngf)), activation]

    if Conv_type == "NC":

    model += [nn.ReflectionPad2d(3), nn.Conv2d(ngf, output_nc,kernel_size=7, padding=0), nn.Tanh()]

    else:

    model += [nn.ReflectionPad2d(3), DEPTHWISECONV(ngf, output_nc, kernel_size=7, padding=0), nn.Tanh()]

    self.model = nn.Sequential(*model)

    def forward(self, input):

    return self.model(input)

    ​

    I successfully transformed them form pytorch into onnx.The first problem about 'list index' arises when I use cubemx. AI to convert the Encoder model,and the problem adout 'params set for InstanceNormalization layer' arises when I use cubemx. AI to convert the Decoder model.

    YYin.2
    Visitor II
    December 3, 2021

    I also have a similar problem. The code is in the attachment.

    Thank you!

    ​