Skip to main content
Evelina CAMILLERI
ST Employee
July 8, 2020
Question

What is the minimum hardware platform needed to develop an algorithm without using the SensorTile.box?

[webinar - Program decision trees in sensors with a Machine Learning Core]

This topic has been closed for replies.

1 reply

Evelina CAMILLERI
ST Employee
July 8, 2020

The minimum hardware required to use the MLC feature is having one of the "X" devices embedding it. Check the following page for more info on the products: https://www.st.com/content/st_com/en/campaigns/machine-learning-core.html. 

The MLC configuration tool available in the Unico GUI can be used offline (without any board) to generate a configuration for one of these devices.

We also provide DIL24 adapter boards of the devices embedding the MLC feature, for instance: STEVAL-MKI195V1, STEVAL-MKI197V1, STEVAL-MKI207V1, STEVAL-MKI210V1K. 

Finally, for further real-time evaluation of the MLC feature, we also provide the STEVAL-MKI109V3 (Professional MEMS Tool) board, which together with the Unico GUI allows a complete evaluation of the MLC feature, from data logging to run-time MLC execution.