Skip to main content
HLU.1
Visitor II
Nov 17, 2022 9:04 AM UTC
Question

What is the compiler when using 'validation on desktop/target' in STM32 Cube AI?

Hey,

If I understand correctly, when using the validation, it will use the upload dl model and c-model to run the inference and then calculate the L2, RMSE, metrics. So I am wondering what the compiler for this is?

Thanks in advance!

This topic has been closed for replies.

1 reply

Semer CHERNI
ST Employee
Nov 18, 2022 10:23 AM UTC

Hello @HLU.1​ 

First let me thank you for posting.

To be able to identify the compiler go to the folder where the pack is installed and execute this command shown below.

This is my case:

C:\Users\the username\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\7.3.0\Utilities\windows\mingw64\bin>gcc.exe --version

gcc.exe (Rev8, Built by MSYS2 project) 11.2.0

Copyright (C) 2021 Free Software Foundation, Inc.

This is free software; see the source for copying conditions. There is NO

warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

You can see it is a GCC compiler.

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.