Associate II
August 7, 2019
Question
Validation on target error timeout error?
- August 7, 2019
- 1 reply
- 1456 views
I'm using STM32L476G-DISCO , running the human activity keras model on Cube MX 5.2 and Using the AI package 4.0.0 , the validation on desktop is successful but I got a "read time error" everytime i run the validation on target also the validation on target runs successfully using the AI Package 3.4.0 ...
Any help? or there still bugs using the package?
this is the report of the validation on the attached file.