Skip to main content
AS.4
Associate
November 25, 2020
Question

Validating custom dataset on STM32 X AI.

Hi

I am following this material to start using STM32 for AI. I have got to the data validation step on page 29 of the document. It works fine while validating using random numbers.

But while trying to validate using the dataset, I get the error:

TOOL ERROR: cannot reshape array of size 1317858 into shape (219643,90,3,1)

Could I please know what should be the validation dataset?

    This topic has been closed for replies.

    3 replies

    Romain LE DONGE
    Associate
    November 25, 2020

    ​Hello,

    What dataset are you using to validate your model ?

    From what I can see, it seems that there is a shape problem in your dataset: (1317858/3 = 439286; 439286/90 = 4880.955 => not an integer), could it be possible that samples are missing maybe ?

    Looking at the shape, it looks like an array of size 59303610 (219643*90*3*1) is required

    Best regards,

    Romain

    AS.4
    AS.4Author
    Associate
    December 7, 2020

    Hi Romain

    I am using a dataset that I collected on-site from a mmWave RADAR.

    I'll check the dataset to determine whether or not samples are missing.

    Could you please recommend the train: test: validate data size ratio that should be used?

    Thank you

    Amogha

    Romain LE DONGE
    Associate
    December 7, 2020

    Hello,

    I'm not a Data Scientist expert and it depends on your data and total dataset size, but I usually use the following split:

    • Training dataset: 60% (70% if I miss data): data to be used to train the network
    • Validation dataset: 20% (10% if I miss data): data to be validated during training process (used to plot train/validation curves)
    • Test dataset: 20%: data to test the final performances of the network (never used during training or network topology research)

    Hope this can help !

    Romain