Skip to main content
Associate II
Aug 22, 2024 3:40 AM UTC
Question

Used Ram over External SDRAM and TFlite Micro runtime

It seems like a used ram size fit to External SDRAM in STM32H757i- EVAL Board.
However, I can see the error when doing analyze.

Also, I cannot see any TFLite Micro runtime generated code.
I can see empty function.
I was totally fine with STM32CUBE AI runtime.

pepsi_zero_sugar_1-1724297824905.png

 

pepsi_zero_sugar_0-1724297679218.png

pepsi_zero_sugar_2-1724297847147.png

pepsi_zero_sugar_3-1724297983155.png

pepsi_zero_sugar_4-1724298006088.png

 

This topic has been closed for replies.

5 replies

fauvarque.daniel
ST Employee
Aug 26, 2024 10:17 AM UTC

You have to select the Template code, System performance application or Validation application to have code generated in those sections

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
Aug 27, 2024 6:39 AM UTC

I selected the Validation application.

I was wondering if TFlite model Used Ram: 1.29MiB, then MCU need x10 size RAM?
It is showing that 1.29 MiB. However, 8 MiB External SDRAM is not enough.

 

fauvarque.daniel
ST Employee
Aug 27, 2024 7:18 AM UTC

with tflite runtime we don't manage automatically the use of external RAM.

That said you can generate the code and modify the linker script to place the activation buffer in external sdram (with of course an impact on the performance)

Regards

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.