Skip to main content
Explorer
February 7, 2024
Question

undefined reference to `ai_emotion_model_create_and_init'

Hi, 

I am trying to create an STM32Cube.AI application using X-Cube-AI. I am following the documentation under Content 6. I trained my own model and configure the .ioc file as shown below. I wanted to get input from the ADC and feed directly into the model to perform classification. I am using the latest X-Cube-AI version 8.1.0. 

goldmine_0-1707289319048.png

Under my X-Cube-AI folder, this is what I got:

goldmine_1-1707289410395.png

I imported my libraries as shown in the documentation.

 

#include "ai_platform.h"
#include "emotion_model.h"
#include "emotion_model_data.h"

 

Then, I created the functions following the documentation.

 

static void AI_Init(void)
{
 ai_error err;

// char buf[50]; // buffer for serial output string
// int buf_len = 0;

 /* Create a local array with the addresses of the activations buffers */
 const ai_handle act_addr[] = { activations };
 /* Create an instance of the model */
 err = ai_emotion_model_create_and_init(&emotion_model, act_addr, NULL);
 if (err.type != AI_ERROR_NONE) {
//	 buf_len = sprintf(buf, "ai_emotion_model_create error - type=%d code=%d\r\n", err.type, err.code);
//	 HAL_UART_Transmit(&huart4, (uint8_t *)buf, buf_len, 100);
	 printf("ai_emotion_model_create error - type=%d code=%d\r\n", err.type, err.code);
	 Error_Handler();
 }
 ai_input = ai_emotion_model_inputs_get(emotion_model, NULL);
 ai_output = ai_emotion_model_outputs_get(emotion_model, NULL);
}

static void AI_Run(float *pIn, float *pOut)
{

 ai_i32 batch;
 ai_error err;

// char buf[50]; // buffer for serial output string
// int buf_len = 0;

 /* Update IO handlers with the data payload */
 ai_input[0].data = AI_HANDLE_PTR(pIn);
 ai_output[0].data = AI_HANDLE_PTR(pOut);

 batch = ai_emotion_model_run(emotion_model, ai_input, ai_output);
 if (batch != 1) {
 err = ai_emotion_model_get_error(emotion_model);
// buf_len = sprintf(buf, "AI ai_emotion_model_run error - type=%d code=%d\r\n", err.type, err.code);
// HAL_UART_Transmit(&huart4, (uint8_t *)buf, buf_len, 100);
 printf("AI ai_emotion_model_run error - type=%d code=%d\r\n", err.type, err.code);
 Error_Handler();
 }
}

 

Basically, I am trying to reproduce the model deployment in STM32MP157F-DK2 on the Cortex-M4 chip with my own model. However, when I was building the project, there are multiple errors as shown:

 

14:54:58 **** Incremental Build of configuration Debug for project emotion_ai_CM4 ****
make -j12 all 
arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DCORE_CM4 -DNO_ATOMIC_64_SUPPORT -DMETAL_INTERNAL -DMETAL_MAX_DEVICE_REGIONS=2 -DVIRTIO_SLAVE_ONLY -DUSE_HAL_DRIVER -DSTM32MP157Fxx -c -I../OPENAMP -I../Core/Inc -I../../Middlewares/Third_Party/OpenAMP/open-amp/lib/include -I../../Middlewares/Third_Party/OpenAMP/libmetal/lib/include -I../../Drivers/STM32MP1xx_HAL_Driver/Inc -I../../Drivers/STM32MP1xx_HAL_Driver/Inc/Legacy -I../../Drivers/CMSIS/Device/ST/STM32MP1xx/Include -I../../Middlewares/Third_Party/OpenAMP/virtual_driver -I../../Drivers/CMSIS/Include -I../../Middlewares/ST/AI/Inc -I../X-CUBE-AI/App -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
arm-none-eabi-gcc -o "emotion_ai_CM4.elf" @"objects.list" -l:NetworkRuntime810_CM4_GCC.a -mcpu=cortex-m4 -T"D:\Nottingham\FYP\Final-Year-Project-Nottingham\code\EMOTION_AI\CM4\STM32MP157FACX_RAM.ld" --specs=nosys.specs -Wl,-Map="emotion_ai_CM4.map" -Wl,--gc-sections -static -L../../Middlewares/ST/AI/Lib -u_printf_float --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-closer.o): in function `_close_r':
(.text._close_r+0xc): warning: _close is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-fstatr.o): in function `_fstat_r':
(.text._fstat_r+0xe): warning: _fstat is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-signalr.o): in function `_getpid_r':
(.text._getpid_r+0x0): warning: _getpid is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-isattyr.o): in function `_isatty_r':
(.text._isatty_r+0xc): warning: _isatty is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-signalr.o): in function `_kill_r':
(.text._kill_r+0xe): warning: _kill is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-lseekr.o): in function `_lseek_r':
(.text._lseek_r+0x10): warning: _lseek is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-readr.o): in function `_read_r':
(.text._read_r+0x10): warning: _read is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(libc_a-writer.o): in function `_write_r':
(.text._write_r+0x10): warning: _write is not implemented and will always fail
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/main.o: in function `AI_Init':
D:/Nottingham/FYP/Final-Year-Project-Nottingham/code/EMOTION_AI/CM4/Debug/../Core/Src/main.c:535: undefined reference to `ai_emotion_model_create_and_init'
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: D:/Nottingham/FYP/Final-Year-Project-Nottingham/code/EMOTION_AI/CM4/Debug/../Core/Src/main.c:542: undefined reference to `ai_emotion_model_inputs_get'
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: D:/Nottingham/FYP/Final-Year-Project-Nottingham/code/EMOTION_AI/CM4/Debug/../Core/Src/main.c:543: undefined reference to `ai_emotion_model_outputs_get'
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Core/Src/main.o: in function `AI_Run':
D:/Nottingham/FYP/Final-Year-Project-Nottingham/code/EMOTION_AI/CM4/Debug/../Core/Src/main.c:559: undefined reference to `ai_emotion_model_run'
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.1.202309131626/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: D:/Nottingham/FYP/Final-Year-Project-Nottingham/code/EMOTION_AI/CM4/Debug/../Core/Src/main.c:561: undefined reference to `ai_emotion_model_get_error'
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:67: emotion_ai_CM4.elf] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.

 

I am not sure what is causing the error since I have included the libraries that has ai_emotion_model_create_and_init as well as ai_emotion_model_run. I have attached the code in my post.

 

Thanks.

This topic has been closed for replies.