Skip to main content
Aalna.1
Associate
Jun 22, 2024 6:08 PM UTC
Question

The inputs for the ML stm32 ai

Hello everyone
I hope someone can help me
I have an ML model that consists of 2 inputs as shown in the picture. Is the code for the inputs correct?

Aalna1_0-1719079464477.png

 

 

 

float ML_input[WINDOW_SIZE*NUM_POINTS];
float Diff_input[WINDOW_SIZE*NUM_POINTS - NUM_POINTS];
static ai_float activations[AI_NETWORK_ADEM_DATA_ACTIVATIONS_SIZE];
static ai_float in_data[AI_NETWORK_ADEM_IN_1_SIZE_BYTES];
static ai_float out_data[AI_NETWORK_ADEM_OUT_1_SIZE_BYTES];
ai_handle adem_network = AI_HANDLE_NULL;
static ai_buffer *ai_input;
static ai_buffer *ai_output;
ai_i32 nbatch;

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_CAN2_Init();
 MX_SPI1_Init();
 MX_USART1_UART_Init();
 MX_CRC_Init();
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 2 */
	Init_A121(); // Init sensor
	ai_network_params ai_params = {AI_NETWORK_ADEM_DATA_WEIGHTS(ai_network_adem_data_weights_get()), AI_NETWORK_ADEM_DATA_ACTIVATIONS(activations)};
	ai_error ai_err;
	ai_input = ai_network_adem_inputs_get(adem_network, NULL);
	ai_output = ai_network_adem_outputs_get(adem_network, NULL);

	ai_err = ai_network_adem_create(&adem_network, AI_NETWORK_ADEM_DATA_CONFIG);
	if(ai_err.type != AI_ERROR_NONE){while(1);}
	if(!ai_network_adem_init(adem_network, &ai_params)){while(1);}

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
	while (1)
	{
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
		Measure_A121();
		DeltaProprocessor(ML_input, Diff_input, NUM_POINTS, WINDOW_SIZE);
		ai_input[0].data = AI_HANDLE_PTR((void*)ML_input);
		ai_input[1].data = AI_HANDLE_PTR((void*)Diff_input);
		ai_output[0].data = AI_HANDLE_PTR(out_data);
		nbatch = ai_network_adem_run(adem_network, &ai_input[0], &ai_output[0]);
	}
 /* USER CODE END 3 */
}

 

 

 

This topic has been closed for replies.