Skip to main content
Associate
Sep 13, 2024 3:15 PM UTC
Solved

Tflite Batch_Matmul and Loop Operator Not Supported

I’m using X-Cube-AI Toolbox 9.1 to realize Vision Transformer deployment but got stuck. I exported from torch using ONNX opset=15. I then used onnx2tf to convert ViT to .tflite format, which is obviously a valid model as shown in Netron. 
1.When I’m trying to analyze it in .tflite, there popped up an error says “BATCH_MATMUL not supported.”
2. Without conversion, analyzing .onnx model popped up something like “tuple has no method get_shape” and failed.

3. I further converted it to .keras and .h5, but .keras says: Unable to load the file, and then the whole CUBE IDE got stuck and expects a restart. Meanwhile .h5 only says something like the Length is four.

All of the trials above deploying ViT model failed with only a single line of error note during model analysis. So I have the following questions:

A) I tried to unroll the matmul in FOR loops, but unfortunately  LOOP operator is also not supported.

 

B) I think one important thing is that the scaled dot product attention module seems to rely heavily on matmul or batch_matmul. So I wonder if the matmul operators, such as @ operator in torch, torch.bmm operator, or torch.einsum, could be supported? Or is there an interface to realize matmul customized operator in X-Cube-AI?

This topic has been closed for replies.
fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Sep 26, 2024 4:10 PM UTC

 Vision Transformer  are currently not supported in STM32Cube.AI 

It is in our development plans but no release date yet.

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Sep 26, 2024 4:10 PM UTC

 Vision Transformer  are currently not supported in STM32Cube.AI 

It is in our development plans but no release date yet.

Regards

Daniel

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.