Skip to main content
Visitor II
April 19, 2026
Question

STm32N6570DK - Hard fault @ 0x24180c5e

Hello ! 

I am trying to build Blinky example on STM32N6570Dk eval board . And this is how my memory.x file looks  like below 


*/
MEMORY
{
FLASH : ORIGIN = 0x24180400, LENGTH = 256K
RAM : ORIGIN = 0x241C0400, LENGTH = 512K
}


When I run cargo run --release , I am getting the error . Could anyone please point what might be the problem here 

 

Running `probe-rs run --chip STM32N657 target/thumbv8m.main-none-eabi/release/blinky`
WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError WARN probe_rs::probe::stlink: send_jtag_command 242 failed: SwdApWdataError Finished in 0.16s
Firmware exited unexpectedly: Exception
Core 0
Frame 0: HardFault_ @ 0x24180c5e
/usr/local/cargo/registry/src/index.crates.io-1949cf8c6b5b557f/cortex-m-rt-0.7.5/src/lib.rs:1103:1
Frame 1: HardFault <Cause: Escalated from an unknown source> @ 0x00000000