Skip to main content
Visitor II
Dec 21, 2025 1:42 AM UTC
Question

STM32N6570-DK E400: Board programming failed!

Hi,

I am working on STM32N6570-DK Edge AI development on Windows and I am facing a board programming error when using stm32ai-modelzoo-services. I would like some guidance on the possible root cause and recommended troubleshooting steps.

Environment

  • Host OS: Windows  11 

  • Board: STM32N6570-DK

  • Tools and versions:

    • STM32CubeProgrammer: v2.20.0 
    • STEdgeAI: 2.2
    • cubeIDE:1.19.0
    • Python: 3.9 

Model and dataset

  • Model: st_yolo_x

  • Dataset: MS COCO 

  • Completed steps:

    • Followed the official instructions to install and configure stm32ai-modelzoo-services on Windows

    • Successfully ran chain_tqeb (training / quantization / evaluation / benchmark) to completion

    • The quantization output folder contains:

      • Quantized model artifacts (e.g. .tflite / .onnx as produced by the pipeline)

      • A user_config file adapted from the official examples

Problem description

  • When running chain_qd or the deployment step for the STM32N6570-DK, the process fails at the “Board programming” stage.

  • The exception I receive is:
    common.stm32ai_local.utils.STMAICToolsError: E400: Board programming failed!

  • At the moment of failure, res_code = -1.

  • From the logs it looks like all model‑related steps (conversion, code generation, project creation) succeed, and only the board programming / flashing step fails.

Attachments

  • I attached a ZIP file that contains:

    • The quantized .tflite model generated from the st_yolo_x network trained on the MS COCO dataset.

This file reflects the exact model I am trying to deploy to the STM32N6570-DK when the E400: Board programming failed! res_code = -1 error occurs.

I will also test with different STM32CubeProgrammer versions on Windows to see whether the programmer version has any impact on this error and will update this thread with my findings.

螢幕擷取畫面 2025-12-21 094025.png

 

 

I would like to add an update based on the solution proposed in

螢幕擷取畫面 2025-12-23 164442.png

螢幕擷取畫面 2025-12-23 164523.png

#850742

Following the suggestion there, I opened the project generated by stm32ai-modelzoo-services in STM32CubeIDE:

...\application_code\object_detection\STM32N6\Application\STM32N6570-DK\STM32CubeIDE

Then I built the project manually in STM32CubeIDE. The build completed successfully with:

  • 0 errors, 0 warnings

  • The following output files present in the Debug folder:

    • STM32N6570-DK_GettingStarted_ObjectDetection.elf

    • STM32N6570-DK_GettingStarted_ObjectDetection.bin

    • STM32N6570-DK_GettingStarted_ObjectDetection_signed.bin

This confirms that the generated project fits in the STM32N6570-DK memory and that the compilation / linking steps are fine. The issue I am still facing is only at the board programming stage when running the deployment chain from the model zoo (I get Board programming failed in the console).

1 reply

Julian E.
ST Technical Moderator
Jan 9, 2026 1:22 PM UTC

Hi @jasonwu,

 

Thank you for this information.

I did successfully deploy your model with model zoo. The only issue I can see is that maybe cubeIDE1.19 could cause the issue; I've seen error due to this version.

 

In any case, I see that you successfully deployed it manually and I don't see anything wrong with what you described/transmitted.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.