Skip to main content
Associate
November 15, 2025
Question

STM32N6570-DK – Deployment stops when ST-LINK is not connected

Dear ST

Environment

Item Version / Details
BoardSTM32N6570-DK
OSUbuntu 24.04 LTS
PythonConda, Python 3.10
STM32AI Model Zoostm32ai-modelzoo-services/object_detection
Operation modedeployment
Modelyolov8n_256_quant_pc_uf_od_coco-person-st.tflite
STM32CubeIDE1.19.0
ST Edge AI Core / STM32CubeAI10.2.0
Local tool/opt/ST/STEdgeAI/2.2/Utilities/linux/stedgeai

Description

I am using the STM32AI Model Zoo deployment workflow on Linux to deploy a YOLOv8 object detection model to the STM32N6570-DK.

The deployment pipeline reaches the final flashing stage and aborts because no ST-LINK device is connected, even though all previous steps (Neural-Art, code generation, project patching) completed successfully.


Console log excerpt

 

 
building.. Debug flashing.. Debug STM32N6570-DK board programming is SKIPPED! -> No valid STM32 development board is connected (ST-LINK/swd port).. ... raise STMAICToolsError('Board programming failed!') E400: Board programming failed!

 

 

Expected behavior

Even when the board is not connected, deployment should still:

  • Finish building the STM32CubeIDE project

  • Export the final firmware (network_data.hex / *.bin)
    This is necessary for CI pipelines and automated batch deployments.


Actual behavior

Because board programming fails due to no ST-LINK detected, the deployment pipeline terminates with an error, and no network_data.hex is produced, even though the Neural-Art and code-gen outputs are valid.

C-project patching is confirmed to be correct:

 

 
network.c network_ecblobs.h network_atonbuf.xSPI2.raw AI_Runtime/

 

 

→ Deployment stops right before final firmware generation.


Current workaround

I manually generate a hex file from network_atonbuf.xSPI2.raw:

 

 
arm-none-eabi-objcopy \ -I binary network_atonbuf.xSPI2.raw \ --change-addresses 0x70380000 \ -O ihex network_data.hex
 

Flashing the resulting hex succeeds, but the display stays completely black (no UI, no bounding boxes, no inference output).
This suggests the manual hex only contains the model blob, not the complete firmware built by the deployment process.


Hypothesis

Deployment performs more than just packing network_atonbuf.xSPI2.raw:

Component Required for successful firmware?
AToN compiled blob✔
application C patching✔
app_config.h update✔
complete CubeIDE project rebuild✔
UI overlay + inference loop✔
ST-LINK programmingshould be optional

Since the deployment aborts before the final firmware build, only the raw model blob is flashed, resulting in a black screen.


Questions for ST

  1. How can we complete the deployment and generate the final firmware (.hex/.bin) without connecting the STM32N6570-DK?

  2. Is there a configuration flag available, e.g.:

    • skip_flasher: true

    • build_only: true

    • generate_hex_without_flashing: true

  3. If the current toolchain does not support this yet, what is the recommended CI-friendly workflow for offline firmware generation?

  4. If the intended solution is “build manually in CubeIDE”, could ST provide documentation on how to:

    • update the project after Neural-Art output

    • trigger a full firmware rebuild

    • avoid black-screen output after flashing

7 replies

Julian E.
ST Technical Moderator
November 17, 2025

Hello @Vic_Ch,

 

Thank you for your detailed post.

It is probably badly explained and not really thought to be used like this, but I think that everything you need in what you describe is present.

 

First, the firmware modified by model zoo services scripts is this package usable as standalone. If you look at the documentation coming with it, it should solve most of your interrogations:

STMicroelectronics/STM32N6-GettingStarted-ObjectDetection: An AI software application package demonstrating simple implementation of object detection use case on STM32N6 product.​

 

If we go back to your situation, even if the deployement is not complete, based on what is being done, you should be able to deploy everything by doing the following:

  1. The default application (the getting started firmware) is in stm32ai-modelzoo-services\application_code\object_detection\STM32N6
  2. in \Model\STM32N6570-DK you should find an updated network_atonbuf.xSPI2.bin, you can either run the command to create the .hex file or directly flash it with CubeProgrammer at this adress: 0x70380000 
    With this, the weights of the model are flashed.
  3. Regarding the app, you need 2 things:
    1. The FSBL, in \binary: ai_fsbl.hex (the source of this is STM32Cube_FW_N6\Projects\STM32N6570-DK\Templates\Template_FSBL_LRUN)
    2. The application with the updated pre and post processing (app_config.h), which you can find in \Application\STM32N6570-DK\STM32CubeIDE\Debug. You can flash STM32N6570-DK_GettingStarted_ObjectDetection_signed.bin at this address: 0x70100000 (found in the doc of the getting started)
  4. If you flash the fsbl, the app and the weights as I described, by restarting the N6 in boot mode, you should have everything functioning correctly.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Vic_ChAuthor
Associate
November 17, 2025

Hi Julia,
I followed the link below and successfully completed the update using the Prebuilt Binaries approach:
https://github.com/STMicroelectronics/STM32N6-GettingStarted-ObjectDetection?tab=readme-ov-file


Question 1
From the following path:
/stm32ai-modelzoo-services/object_detection/src/experiments_outputs/2025_11_17_21_55_57/generated
Can I directly create STM32N6570-DK/network_data.hex to replace the current model and proceed with flashing?

截圖 2025-11-18 清晨6.33.52.png
Question 2
Is it possible to package the model solely using the following shell script?
https://github.com/STMicroelectronics/stm32ai-modelzoo-services/blob/main/application_code/object_detection/STM32N6/Model/generate-n6-model_STM32N6570-DK.sh


Question 3
If I want a single project to include multiple models, is that feasible?


Question 4
Ultimately, I would like to separate model generation and firmware development into two independent workflows (traditional development flow).
Is this achievable?

Julian E.
ST Technical Moderator
November 19, 2025

Hi @Vic_Ch,

 

1) I don't remember exactly what is replaced, but yes, it takes files from the experiment_outputs and replace them in the application being flashed. Look at the files date in /application_code to know what is from the default getting started and what was replaced.

 

2) The getting started application were designed to be use as standalone (manually or with the .sh scripts) or via the model zoo. In the end it is the same thing, so yes, you can just use the shell scripts.

 

3) yes, you can, I believe that the hand landmark package uses one model for the detection of the hand on the image, then a second one for the landmarks: STM32N6-AI | Software - STMicroelectronics

This document should also be helpful: ST Neural-ART NPU concepts

 

4) These documents present what to take into considaration, but as long as you have that in mind and keep in mind the memory needed for the activations and weights of the model (result of the generate command, using the st edge ai core), then, yes I think it answers your needs.

STM32N6 Example projects & tips for creating new projects

Session - ST Edge AI Developer Cloud

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.