Skip to main content
Visitor II
Feb 27, 2026 5:31 PM UTC
Question

STM32H753ZI and NanoEdgeAI

I wanted to run ready-made examples for the STM32H753ZI in NanoEdge AI but I couldn't find any. Does anyone have any tips or a ready-made example?

1 reply

Julian E.
ST Technical Moderator
Mar 4, 2026 1:17 PM UTC

Hi @LucasCalsing,

 

I don’t think there is an example specifically for this board.

NanoEdge AI libraries are straightforward to integrate and are not dependent on a particular hardware platform.

I recommend looking at:

AI:How to Build an Anomaly Detection Project for Predictive Maintenance with NanoEdge AI Studio - stm32mcu

(This is for Anomaly detection, but for all project, the idea is pretty much the same)

 

The simplest POC you can build is to:

  1. Create an MX project for your board with the default settings.
  2. In main, allocate a buffer matching the size of the data you used in NanoEdge.
    (You can put random values inside)
  3. After including the NanoEdge library, call:
    • an initialization function,
    • optionally a learning function if you are doing anomaly detection,
    • and then the inference function.
  4. Finally print the result

And that’s all you need for a basic proof of concept.

 

Then you would need to configure your sensor and continue your project

 

You can also look at the example datalogger we published.
I believe all example are doing both datalogging and a simple prediction loop:

GitHub - stm32-hotspot/stm32ai-nanoedge-datalogger: STM32 Application for datalogging feature with NanoEdge AI Studio · GitHub

 

Have a good day,

Julian

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.