Skip to main content
Associate
Sep 23, 2024 12:20 PM UTC
Solved

stm32h750 x-cube-ai , ai_network_create_and_init() code stuck

Snipaste_2024-09-23_20-19-02.jpg

This topic has been closed for replies.
FuShenXiaoBest answer
Visitor II
Sep 30, 2024 7:34 AM UTC

I have already enabled the CRC IP by adding "__HAL_RCC_CRC_CLK_ENABLE();" before "AI_Init();" but still have the log "ai_network_create error - type=51 code=65"

The following is a part of my main.c file

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "string.h"
#include "ai_platform.h"
#include "network.h"
#include "network_data.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

CRC_HandleTypeDef hcrc;

UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_CRC_Init(void);
static void MX_FLASH_Init(void);
static void MX_UART4_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

int fputc(int ch, FILE *f)
{
 HAL_UART_Transmit(&huart4, (uint8_t *)&ch, 1, 0xffff);
 return ch;
}

int fgetc(FILE *f)
{
 uint8_t ch = 0;
 HAL_UART_Receive(&huart4, &ch, 1, 0xffff);
 return ch;
}

ai_handle network;
float aiInData[AI_NETWORK_IN_1_SIZE];
float aiOutData[AI_NETWORK_OUT_1_SIZE];
ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];

ai_buffer * ai_input;
ai_buffer * ai_output;

static void AI_Init(void);
static void AI_Run(float *pIn, float *pOut);
void PictureCharArrayToFloat(uint8_t *srcBuf,float *dstBuf,int len);


void Uart_send(char * str);
#define UART_BUFF_LEN 1024
#define ONE_FRAME_LEN 1+784+2
uint16_t uart_rx_length = 0;
uint8_t uart_rx_byte = 0;
uint8_t uart_rx_buffer[UART_BUFF_LEN];
volatile uint8_t goRunning = 0;
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Update SystemCoreClock variable according to RCC registers values. */
 SystemCoreClockUpdate();

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_CRC_Init();
 MX_FLASH_Init();
 MX_UART4_Init();
 /* USER CODE BEGIN 2 */
 __HAL_RCC_CRC_CLK_ENABLE();
 AI_Init();
 memset(uart_rx_buffer,0,784);
 HAL_UART_Receive_IT(&huart4, (uint8_t *)&uart_rx_byte, 1);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 char str[10];
	 if(goRunning>0)
	 {
	 if(uart_rx_length == ONE_FRAME_LEN)
	 {
	 PictureCharArrayToFloat(uart_rx_buffer+1,aiInData,28*28);
	 AI_Run(aiInData, aiOutData);
	 }
	 memset(uart_rx_buffer,0,784);
	 goRunning = 0;
	 uart_rx_length = 0;
	 }
 }
 /* USER CODE END 3 */
}

/**
 * @brief CRC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 hcrc.Instance = CRC;
 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}

/**
 * @brief FLASH Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_FLASH_Init(void)
{

 /* USER CODE BEGIN FLASH_Init 0 */

 /* USER CODE END FLASH_Init 0 */

 /* USER CODE BEGIN FLASH_Init 1 */

 /* USER CODE END FLASH_Init 1 */
 /* USER CODE BEGIN FLASH_Init 2 */

 /* USER CODE END FLASH_Init 2 */

}

/**
 * @brief UART4 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UART4_Init(void)
{

 /* USER CODE BEGIN UART4_Init 0 */

 /* USER CODE END UART4_Init 0 */

 /* USER CODE BEGIN UART4_Init 1 */

 /* USER CODE END UART4_Init 1 */
 huart4.Instance = UART4;
 huart4.Init.BaudRate = 115200;
 huart4.Init.WordLength = UART_WORDLENGTH_8B;
 huart4.Init.StopBits = UART_STOPBITS_1;
 huart4.Init.Parity = UART_PARITY_NONE;
 huart4.Init.Mode = UART_MODE_TX_RX;
 huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart4.Init.OverSampling = UART_OVERSAMPLING_16;
 huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART4_Init 2 */

 /* USER CODE END UART4_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 __HAL_RCC_GPIOM_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
	if(goRunning ==0)
	{
		if (uart_rx_length < UART_BUFF_LEN)
		{
			uart_rx_buffer[uart_rx_length] = uart_rx_byte;
			uart_rx_length++;

			if (uart_rx_byte == '\n')
			{
				goRunning = 1;
			}
		}
		else
		{
			//rt_kprintf("rx len over");
			uart_rx_length = 0;
		}
	}
	HAL_UART_Receive_IT(&huart4, (uint8_t *)&uart_rx_byte, 1);
}

void Uart_send(char * str)
{
	HAL_UART_Transmit(&huart4, (uint8_t *)str, strlen(str),0xffff);
}

static void AI_Init(void)
{
 ai_error err;

 /* Create a local array with the addresses of the activations buffers */
 const ai_handle act_addr[] = { activations };
 /* Create an instance of the model */
 err = ai_network_create_and_init(&network, act_addr, NULL);
 if (err.type != AI_ERROR_NONE) {
 printf("ai_network_create error - type=%d code=%d\r\n", err.type, err.code);
 Error_Handler();
 }
 ai_input = ai_network_inputs_get(network, NULL);
 ai_output = ai_network_outputs_get(network, NULL);
}

static void AI_Run(float *pIn, float *pOut)
{
	char logStr[100];
	int count = 0;
	float max = 0;
 ai_i32 batch;
 ai_error err;

 /* Update IO handlers with the data payload */
 ai_input[0].data = AI_HANDLE_PTR(pIn);
 ai_output[0].data = AI_HANDLE_PTR(pOut);

 batch = ai_network_run(network, ai_input, ai_output);
 if (batch != 1) {
 err = ai_network_get_error(network);
 printf("AI ai_network_run error - type=%d code=%d\r\n", err.type, err.code);
 Error_Handler();
 }
 for (uint32_t i = 0; i < AI_NETWORK_OUT_1_SIZE; i++) {

	 sprintf(logStr,"%d %8.6f\r\n",i,aiOutData[i]);
	 Uart_send(logStr);
	 if(max<aiOutData[i])
	 {
		 count = i;
		 max= aiOutData[i];
	 }
 }
 sprintf(logStr,"current number is %d\r\n",count);
 Uart_send(logStr);
}

void PictureCharArrayToFloat(uint8_t *srcBuf,float *dstBuf,int len)
{
	for(int i=0;i<len;i++)
	{
		dstBuf[i] = srcBuf[i];//==1?0:1;
	}
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

Best Regards

3 replies

fauvarque.daniel
ST Employee
Sep 26, 2024 4:05 PM UTC

You probably didn't enable the CRC IP in your application

Regards

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
FuShenXiaoBest answer
Visitor II
Sep 30, 2024 7:34 AM UTC

I have already enabled the CRC IP by adding "__HAL_RCC_CRC_CLK_ENABLE();" before "AI_Init();" but still have the log "ai_network_create error - type=51 code=65"

The following is a part of my main.c file

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "stdio.h"
#include "string.h"
#include "ai_platform.h"
#include "network.h"
#include "network_data.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

CRC_HandleTypeDef hcrc;

UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_CRC_Init(void);
static void MX_FLASH_Init(void);
static void MX_UART4_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

int fputc(int ch, FILE *f)
{
 HAL_UART_Transmit(&huart4, (uint8_t *)&ch, 1, 0xffff);
 return ch;
}

int fgetc(FILE *f)
{
 uint8_t ch = 0;
 HAL_UART_Receive(&huart4, &ch, 1, 0xffff);
 return ch;
}

ai_handle network;
float aiInData[AI_NETWORK_IN_1_SIZE];
float aiOutData[AI_NETWORK_OUT_1_SIZE];
ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];

ai_buffer * ai_input;
ai_buffer * ai_output;

static void AI_Init(void);
static void AI_Run(float *pIn, float *pOut);
void PictureCharArrayToFloat(uint8_t *srcBuf,float *dstBuf,int len);


void Uart_send(char * str);
#define UART_BUFF_LEN 1024
#define ONE_FRAME_LEN 1+784+2
uint16_t uart_rx_length = 0;
uint8_t uart_rx_byte = 0;
uint8_t uart_rx_buffer[UART_BUFF_LEN];
volatile uint8_t goRunning = 0;
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Update SystemCoreClock variable according to RCC registers values. */
 SystemCoreClockUpdate();

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_CRC_Init();
 MX_FLASH_Init();
 MX_UART4_Init();
 /* USER CODE BEGIN 2 */
 __HAL_RCC_CRC_CLK_ENABLE();
 AI_Init();
 memset(uart_rx_buffer,0,784);
 HAL_UART_Receive_IT(&huart4, (uint8_t *)&uart_rx_byte, 1);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 char str[10];
	 if(goRunning>0)
	 {
	 if(uart_rx_length == ONE_FRAME_LEN)
	 {
	 PictureCharArrayToFloat(uart_rx_buffer+1,aiInData,28*28);
	 AI_Run(aiInData, aiOutData);
	 }
	 memset(uart_rx_buffer,0,784);
	 goRunning = 0;
	 uart_rx_length = 0;
	 }
 }
 /* USER CODE END 3 */
}

/**
 * @brief CRC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_CRC_Init(void)
{

 /* USER CODE BEGIN CRC_Init 0 */

 /* USER CODE END CRC_Init 0 */

 /* USER CODE BEGIN CRC_Init 1 */

 /* USER CODE END CRC_Init 1 */
 hcrc.Instance = CRC;
 hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;
 hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE;
 hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;
 hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;
 hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;
 if (HAL_CRC_Init(&hcrc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CRC_Init 2 */

 /* USER CODE END CRC_Init 2 */

}

/**
 * @brief FLASH Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_FLASH_Init(void)
{

 /* USER CODE BEGIN FLASH_Init 0 */

 /* USER CODE END FLASH_Init 0 */

 /* USER CODE BEGIN FLASH_Init 1 */

 /* USER CODE END FLASH_Init 1 */
 /* USER CODE BEGIN FLASH_Init 2 */

 /* USER CODE END FLASH_Init 2 */

}

/**
 * @brief UART4 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_UART4_Init(void)
{

 /* USER CODE BEGIN UART4_Init 0 */

 /* USER CODE END UART4_Init 0 */

 /* USER CODE BEGIN UART4_Init 1 */

 /* USER CODE END UART4_Init 1 */
 huart4.Instance = UART4;
 huart4.Init.BaudRate = 115200;
 huart4.Init.WordLength = UART_WORDLENGTH_8B;
 huart4.Init.StopBits = UART_STOPBITS_1;
 huart4.Init.Parity = UART_PARITY_NONE;
 huart4.Init.Mode = UART_MODE_TX_RX;
 huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart4.Init.OverSampling = UART_OVERSAMPLING_16;
 huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
 huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART4_Init 2 */

 /* USER CODE END UART4_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();
 __HAL_RCC_GPIOM_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
	if(goRunning ==0)
	{
		if (uart_rx_length < UART_BUFF_LEN)
		{
			uart_rx_buffer[uart_rx_length] = uart_rx_byte;
			uart_rx_length++;

			if (uart_rx_byte == '\n')
			{
				goRunning = 1;
			}
		}
		else
		{
			//rt_kprintf("rx len over");
			uart_rx_length = 0;
		}
	}
	HAL_UART_Receive_IT(&huart4, (uint8_t *)&uart_rx_byte, 1);
}

void Uart_send(char * str)
{
	HAL_UART_Transmit(&huart4, (uint8_t *)str, strlen(str),0xffff);
}

static void AI_Init(void)
{
 ai_error err;

 /* Create a local array with the addresses of the activations buffers */
 const ai_handle act_addr[] = { activations };
 /* Create an instance of the model */
 err = ai_network_create_and_init(&network, act_addr, NULL);
 if (err.type != AI_ERROR_NONE) {
 printf("ai_network_create error - type=%d code=%d\r\n", err.type, err.code);
 Error_Handler();
 }
 ai_input = ai_network_inputs_get(network, NULL);
 ai_output = ai_network_outputs_get(network, NULL);
}

static void AI_Run(float *pIn, float *pOut)
{
	char logStr[100];
	int count = 0;
	float max = 0;
 ai_i32 batch;
 ai_error err;

 /* Update IO handlers with the data payload */
 ai_input[0].data = AI_HANDLE_PTR(pIn);
 ai_output[0].data = AI_HANDLE_PTR(pOut);

 batch = ai_network_run(network, ai_input, ai_output);
 if (batch != 1) {
 err = ai_network_get_error(network);
 printf("AI ai_network_run error - type=%d code=%d\r\n", err.type, err.code);
 Error_Handler();
 }
 for (uint32_t i = 0; i < AI_NETWORK_OUT_1_SIZE; i++) {

	 sprintf(logStr,"%d %8.6f\r\n",i,aiOutData[i]);
	 Uart_send(logStr);
	 if(max<aiOutData[i])
	 {
		 count = i;
		 max= aiOutData[i];
	 }
 }
 sprintf(logStr,"current number is %d\r\n",count);
 Uart_send(logStr);
}

void PictureCharArrayToFloat(uint8_t *srcBuf,float *dstBuf,int len)
{
	for(int i=0;i<len;i++)
	{
		dstBuf[i] = srcBuf[i];//==1?0:1;
	}
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

Best Regards

winkAuthor
Associate
Oct 3, 2024 4:28 AM UTC

I have identified the issue, which is that printf forgot to redirect and the PLL settings generated automatically by cubemx are incorrect. These two errors were mixed together and caused