Skip to main content
BKOSI.1
Associate III
May 26, 2021
Question

[STM32H745I-DISCO] Validation on target

Hi,

I've some questions about validation on target, we meet some issues.

Two ways are offer to do that, with or without automatic generate, compile, etc.

1 - We tried the second method, and code generation stop due to not enough internal RAM. We are not able to modify STM32H745XI.ld to change AXI-SRAM lenght from 256KB to 512KB due to automatic code generation and we don't know local directory used for this method.

Can we make a workarround if we decide to use external SRAM for neural network ?

2 - We tried first method and build, program targets following AN5361 for configuration.

We build project as debug application, however CubeMX can't find eval board for validation on target.

3 - Last question about performance validation, we only select "Performance" on X-Cube-AI Device Application menu ?

Thanks you for your support,

BR

Benjamin

This topic has been closed for replies.

2 replies

BKOSI.1
BKOSI.1Author
Associate III
May 31, 2021

Hi community,

Someone can help us ?

We tried with validation and performance application, same results.

No communication between board and CubeMX or TeraTerm.

BR,

Benjamin

BKOSI.1
BKOSI.1Author
Associate III
June 3, 2021

Hi,

After few tests i' able to :

  • M4 & M7 Registers access through Cubeprogrammer
  • Access to M4 debug through M7 access
  • STlinV3 up to date
  • NRST connected to STLink reset

So maybe I brick M4 access port or STlink ?

I will appreciate a support from STemployee if possible... or someone else who meet this situation.

BR

Benjami