Skip to main content
SEMEH_SAYADI
Explorer
Aug 1, 2024 2:55 PM UTC
Solved

STM32CubeFunctionPack_DATALOG2_V2.1.0

I was trying to reconfigure and customize the HMI given by HSDATALOG2 interface , i have been looking into utilities/HSDPython_SDK/examples ; utilities/HSDPython_SDK/st_dtdl_gui but i can't see how i can manage the controll over the widgets colours and texts .

i' ve consulted the scripts written in python , JSON files but nothing changes while executing the main .

is there a file that contains all the widgets , how may i make my own changements.

 

SEMEH_SAYADI_0-1722523959802.png

 

 

@SimonePradolini
@Federica Bossi 
This topic has been closed for replies.
SimonePradolini
SimonePradoliniBest answer
ST Technical Moderator
Sep 4, 2024 8:06 AM UTC

Hello @SEMEH_SAYADI 

Sorry for the late reply. The tag you inserted didn't work properly, so I wasn't notified about your request.

HSDPython_SDK is based on wheel packages installed through the provided installer. The source code is also released, and you are free to have a look at it, but the code running is related to the already-packaged wheel. So, you must act in the path where you installed our packages. Where did you install the SDK? Have you enabled a virtual environment before installing the SDK?

If so, the source code to modify is in your virtual environment under \Lib\site-packages\ (e.g., I built the virtual environment called .venv in the root folder of the SDK, so the code is in \Utilities\HSDPython_SDK\.venv\Lib\site-packages\st_dtdl_gui). If not, the package has been installed in your system Python home folder.

Widgets are divided into types: there is a file for each kind of widget (e.g., plots are organized into Lines, Heatmaps, Bars, etc.).

Best regards,
Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

SimonePradolini
SimonePradoliniBest answer
ST Technical Moderator
Sep 4, 2024 8:06 AM UTC

Hello @SEMEH_SAYADI 

Sorry for the late reply. The tag you inserted didn't work properly, so I wasn't notified about your request.

HSDPython_SDK is based on wheel packages installed through the provided installer. The source code is also released, and you are free to have a look at it, but the code running is related to the already-packaged wheel. So, you must act in the path where you installed our packages. Where did you install the SDK? Have you enabled a virtual environment before installing the SDK?

If so, the source code to modify is in your virtual environment under \Lib\site-packages\ (e.g., I built the virtual environment called .venv in the root folder of the SDK, so the code is in \Utilities\HSDPython_SDK\.venv\Lib\site-packages\st_dtdl_gui). If not, the package has been installed in your system Python home folder.

Widgets are divided into types: there is a file for each kind of widget (e.g., plots are organized into Lines, Heatmaps, Bars, etc.).

Best regards,
Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
SimonePradolini
ST Technical Moderator
Sep 13, 2024 7:31 AM UTC

Hello @SEMEH_SAYADI 

Can you please click on Accept as Solution if you are satisfied or come back to us with any further request?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.