Skip to main content
Associate
Apr 29, 2025 4:25 AM UTC
Question

STM32CubeAI: INTERNAL ERROR: E801(HwIOError): Invalid firmware

Dear Community,

I am attempting to deploy an .onnx model to STM32F407VET6 via STM32CubeAI 10.0.0.

I have generated the code, completed the compilation and download through MDK5, and also completed the validate on desktop on STM32CubeMX. However, when conducting the validate on target, I encountered the "INTERNAL ERROR: E801(HwIOError): Invalid firmware - COM3:115200" issue. I'm a novice, maybe I haven't done the configuration work well and don't know how to make adjustments.


I have attached my code file in the attachment. If I need to provide more relevant files, please let me know. I would be extremely grateful!

 

Regards

knight

This topic has been closed for replies.

3 replies

Julian E.
ST Technical Moderator
Apr 29, 2025 8:29 AM UTC

Hello @knight,

 

To do a validation target with X Cube AI:

  • Make sure to use the lastest available version of X Cube AI
  • Open CubeMX and select your board

JulianE_5-1745915306567.png

  • Initialize all peripherals as default
  • Look for X Cube AI under Middleware and Software Packs
  • Activate X Cube AI and select the validation template

JulianE_4-1745915262744.png

  • Browse for your model
  • Make sure that the model is compatible by doing an Analysis
  • Click on Validation on Target
  • Com Port: Automatic, Baudrate: 115200 (921600 for N6)
  • Check Automatic Compilation and Download
  • Select your toolchain / IDE: STM32CubeIDE
  • Make sure that your board is connected to the PC

JulianE_3-1745915245825.png

 

Then, to create your own application, use the application template instead of the validation template

 

Have a good day,

Julian

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
knightAuthor
Associate
Apr 30, 2025 2:16 AM UTC

Dear Julian,

 

Thanks for the guideline! I followed your steps, successfully generated code in STM32CubeMX, built and run project in STM32CubeIDE, but when I tried to validate on target again, there is a "No board connected on the machine with MCU" issue. Do you know how to fix it? Thanks a lot again.Shutting down.jpg

 

No board connected on the machine with MCU .jpg

Regards

knight

Bartosz BORYNA
ST Employee
May 5, 2025 6:17 AM UTC

Dear Knight,

In order to perform validation on target you need connection to MCU UART via ST-Link Virtual COM Port (VCP) to exchange validation data with PC e.g. on NUCLEO board such a connection is implemented. I'm not sure what kind of STM32F407 board you are using (proprietary one ?), please make sure you have such a connection and ST-Link is capable to provide VCP profile (>= ST-Link v2.1). As reference you can see NUCLEO-F429 -> USART3 pins PD8, PD9 are connected to on-board ST-Link VCP.

 

Best regards,

Bartosz