Skip to main content
Visitor II
Nov 23, 2026 4:14 PM UTC
Question

STM32Cube AI Studio Validation Error on L4R5ZI (E200(ValidationError) / E801(HwIOError) / Unable to bind the ST.AI runtime)

Hi,

I'm working on a project in STM32Cube AI Studio for the L4R5ZI board, using a ResNet8 model (int8 version from MLPerf Tiny for the CIFAR10 dataset) with default settings. During model validation on the target, I encounter the following error:

INFO   [ST Edge AI Core] Running the ST.AI c-model (AI RUNNER)...(name=network, mode=TARGET)INFO   [ST Edge AI Core] E200(ValidationError): TARGET: Unable to bind the ST.AI runtime with "network" c-model: []INFO   [ST Edge AI Core]  E801(HwIOError): Invalid firmware - COM10:115200INFO   Command for ST Edge AI Core finishedERROR   Command for ST Edge AI Core failed, return code 4294967295INFO   Target 0670FF525282494867194720 releasedERROR   Error during run, due to ST Edge AI Core error. TARGET: Unable to bind the ST.AI runtime with "network" c-model: []INFO   Tasks: usb [STM32CubeProgrammer v2.23.0], analyze [ST Edge AI Core v4.1.0], generate [ST Edge AI Core v4.1.0], download_pack [STM32CubeMX v6.19.0], create_project [STM32CubeMX v6.19.0], generate_project [STM32CubeMX v6.19.0], copy_flasher [STM32CubeProgrammer v2.23.0], copy_external_memory_deps [STM32CubeMX v6.19.0], main_updater [STM32CubeMX v6.19.0], build [CMake v4.3.2], usb [STM32CubeProgrammer v2.23.0], flash [STM32CubeProgrammer v2.23.0], validate [ST Edge AI Core v4.1.0]

 

See attached failed log.

 

Additional details:

  • The error occurs with both CMake and CubeIDE toolchains.
  • The board firmware is updated to the latest version (V2J48M35).
  • The error persists regardless of the CubeMX "Prefer online templates when available" setting.

 

Thanks