Skip to main content
Associate II
September 26, 2026
Question

Stm32cube ai studio can't run my inference on my NUCLEO-N657X0-Q - Error: failed to erase memory

Stm32cubeAI studio output


      -------------------------------------------------------------------

                       STM32CubeProgrammer v2.23.0                  
      -------------------------------------------------------------------


ST-LINK SN  : 0042001A3234510337333934

ST-LINK FW  : V3J17M10
Board       : NUCLEO-N657X0-Q
Voltage     : 3.30V

SWD freq    : 8000 KHz

Connect mode: Under Reset
Reset mode  : Hardware reset

Device ID   : 0x486

Revision ID : Rev Z

Device name : STM32N6xx
Device type : MCU
Device CPU  : Cortex-M55
BL Version  : --


Opening and parsing file: NUCLEO-N657X0-Q_Appli.elf

Memory Programming ...
  File          : NUCLEO-N657X0-Q_Appli.elf

  Size          : 2.60 MB 
  Address       : 0x34000000

Erasing memory corresponding to segment 0:
Erasing memory corresponding to segment 1:

Erasing external memory sectors [16 57]

Error: failed to erase memory


Error: failed to erase memory

Run failed: Error: STM32CubeProgrammer exited with code 1
 

1 reply

Julian E.
ST Technical Moderator
September 29, 2026

Hi ​@Monssef,

 

Is your BOOT0 at high (1)?

Make sure to do a power reset.

 

Please also make sure in the STM32Cube AI Studio settings that the version of cubeprogrammer meets the requirements.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.