Skip to main content
Associate II
Mar 24, 2025 8:40 AM UTC
Question

STM32 model zoo help

Im trying to deploy an audio detection model i trained and developed using yamnet onto the B-U585I-IOT02A board that differentiates between normal and abnormal machine sounds. I am trying to implement the AI on stm32cubeide but dont know how to do it. I saw a freertos guide or something but dont really know how to implement or use it? 

 

This topic has been closed for replies.

8 replies

jzzunnAuthor
Associate II
Mar 24, 2025 12:52 PM UTC

Duplicate - merged.


I get this error when trying to open the .ioc file. I opened the project of freertos from stm32 model zoo for audio. 

Invalid Input: Must be project's active .ioc file.

Project's 'Projects' active one is 'Projects.ioc' file

Julian E.
ST Technical Moderator
Mar 24, 2025 2:57 PM UTC

Hello @jzzunn 

 

it seems that you use the ST Model Zoo.

In this case, please look at this tutorial on how to deploy a model on a B-U585I-IOT02A

stm32ai-modelzoo-services/audio_event_detection/deployment/README.md at main · STMicroelectronics/stm32ai-modelzoo-services

 

If you have any issues following this tutorial, feel free to reach out to me!

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jzzunnAuthor
Associate II
Mar 24, 2025 3:36 PM UTC

I dont want to use the deployment tutorial because i am trying to do it with my own model file that i converted using stm32 cloud ai

 

Julian E.
ST Technical Moderator
Mar 24, 2025 4:12 PM UTC

First, you can deploy your own model with it. Model Zoo will generate the same files as Stm32 Dev Cloud did.

Then, about your ioc issue, where did you get this file?

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jzzunnAuthor
Associate II
Mar 24, 2025 4:37 PM UTC

I just added the project from the freertos folder of stm32 model zoo didnt change anything, but i think it was because the ioc file was placed outside the actual project for some reason

 

jzzunnAuthor
Associate II
Mar 24, 2025 4:33 PM UTC

This is my model, the feature extraction layers uses YAMNet's pretrained feature extraction and adding my own classification layers on top:

def extract_features(audio_file, sample_rate=16000:(
    """Extract YAMNet embeddings from an audio file"""
    # Load audio file
    audio, sr = librosa.load(audio_file, sr=sample_rate, mono=True)
   
    # Ensure audio is the right length (at least 1 second)
    if len(audio) < sample_rate:
        audio = np.pad(audio, (0, sample_rate - len(audio)))
   
    # Get YAMNet embeddings
    yamnet_model = hub.load('https://tfhub.dev/google/yamnet/1')
    scores, embeddings, _ = yamnet_model(audio)
   
    return embeddings
 
Class YAMNetTransferModel:
def __init__(self:(
        # Load the YAMNet model from TensorFlow Hub
        self.yamnet_model = hub.load('https://tfhub.dev/google/yamnet/1')
        self.input_shape = (None, 1024)  # YAMNet embeddings shape
       
        # Build the classifier model on top of YAMNet embeddings
        self.model = self._build_model()
   
    def _build_model(self:(
        """Build a classifier on top of YAMNet embeddings"""
        # Input layer for YAMNet embeddings
        inputs = keras.layers.Input(shape=self.input_shape)
       
        # Add layers for classification
        x = keras.layers.GlobalAveragePooling1D()(inputs)
        x = keras.layers.Dense(128, activation='relu')(x)
        x = keras.layers.Dropout(0.3)(x)
        x = keras.layers.Dense(64, activation='relu')(x)
        x = keras.layers.Dropout(0.2)(x)
        outputs = keras.layers.Dense(2, activation='softmax')(x)  # 2 classes: normal and anomalous
       
        # Create and compile the model
        model = keras.Model(inputs=inputs, outputs=outputs)
        model.compile(
            optimizer=keras.optimizers.Adam(learning_rate=0.001),
            loss='sparse_categorical_crossentropy',
            metrics=['accuracy']
        )
       
        return model
jzzunnAuthor
Associate II
Mar 24, 2025 4:49 PM UTC

How do i implement this model to the custom_model.py code because i dont have feature extraction layers, im just importing yamnet's feature extraction from tensorflowhub. Besides, Im trying to develop a webserver that can deploy models to the stm32 board from the server itself so i would prefer not to use model zoo config files etc because it is not very user friendly 

Julian E.
ST Technical Moderator
Mar 25, 2025 9:13 AM UTC

Hello @jzzunn ,

 

I think that the best way for you to deploy your model is to use X Cube AI from STM32CubeMX.

Take a look at this document: UM2526Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI) (https://www.st.com/en/embedded-software/x-cube-ai.html#documentation)

 

With this, you should be able to generate a template application that run an inference of your model with a random input and outputs via serial some metrics.

 

In the generated code, the API related to AI is explained here:

https://stedgeai-dc.st.com/assets/embedded-docs/embedded_client_api_legacy.html 

 

Have a good day,

Julian

 

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.