Skip to main content
Associate II
Mar 17, 2026 6:12 PM UTC
Question

STM32 Cube AI Studio FP32 Model Compilation Issue

Hi

I have FP32 TFLite model. I can able to compile quantised model with STM32 Cube AI studio. i am getting some error while compiling FP32 model with STM32 Cube AI studio. Please let me know the steps to build FP32 model and make the C files correspond to the model.

 

3 replies

Julian E.
ST Technical Moderator
Mar 18, 2026 9:36 AM UTC

Hi @RanjithRemasan,

 

What is the error that you get?

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
Mar 18, 2026 3:12 PM UTC

HI @Julian E. 

 

Please see the error log. i have tried to compile Resnet8 

 

ST_AI_Error.png

Julian E.
ST Technical Moderator
Mar 23, 2026 9:41 AM UTC

Hi @RanjithRemasan, 

 

Could you share your model (in a .zip)?

Based on the error message it seems that the st edge ai core fails to replace your float32 input to a uint8 one (in the .sh, in the generate command you have "--input-data-type uint8")

 

I tried it with our resnet8 and got no issue.

stm32ai-modelzoo/image_classification/resnet/ST_pretrainedmodel_public_dataset/cifar10/resnet8_32_tfs at main · STMicroelectronics/stm32ai-modelzoo · GitHub

 

This model has a uint8 input, unlike your model. Maybe it causes the issue.

But it would be strange that it fails to replace the float32 input as the "--input-data-type uint8" is made for that...

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.