ST EdgeAI Core run model validation on stm32mp257, missing information 'inference time for each node'
- 2 replies
- 563 views
Hello
I want to use ST Edge AI Core for model validate on STM32MP257.
When I set the parameter --mode host, the report results include "Inference time per node"
command: stedgeai validate -m ./linear_model_quantized.onnx --target stm32mp2 --mode host -v 2
part of report result:
Inference time per node
---------------------------------------------------------------------------
c_id m_id type dur (ms) % cumul name
---------------------------------------------------------------------------
0 0 NL (0x107) 0.001 30.8% 30.8% ai_node_0
1 18 Dense (0x104) 0.001 30.8% 61.5% ai_node_1
2 18 NL (0x107) 0.001 26.9% 88.5% ai_node_2
---------------------------------------------------------------------------
n/a n/a Inter-nodal 0.000 11.5% 100.0% n/a
---------------------------------------------------------------------------
total 0.003
---------------------------------------------------------------------------
But I want to see the actual inference time of each layer of the model running on NPU.
So, I run command: stedgeai validate -m ./linear_model_quantized.onnx --target stm32mp2 --mode target -d mpu:192.168.0.10:npu -v 2
report is in attach files,without infomation "Inference time per node"
Is it because the validation on STM32MP257 does not support "Inference time per node", or did I use incorrect tool parameters or firmware version?
Thanks