Skip to main content
Associate
Jul 29, 2025 6:52 PM UTC
Question

Sharing my repo - Multi-Model Face Recognition Pipeline on STM32N6

 

I've implemented a multi-model face recognition system on the STM32N6 (originally based on the single model object detection demo) that efficiently runs detection and recognition models simultaneously on the NPU. Sharing the complete implementation since deploying and managing multiple AI models on the hardware has some non-obvious challenges.

  • Detection Model: CenterFace for face detection (9ms inference)
  • Recognition Model: MobileFaceNet (130ms per face)
  • Pipeline Management: Efficient switching between models on the NPU
  • Automated Deployment: Script that takes model paths, names, and addresses as JSON elements and builds + flashes them automatically

Repository: https://github.com/PeleAB/STM32N6-FaceRecognition

Next steps include creating an abstraction layer for JPEG and H264 compression to handle video streams more efficiently.

Happy to discuss multi-model deployment strategies or NPU optimization approaches. The automated build system alone might save others significant setup time.

This topic has been closed for replies.

2 replies

Julian E.
ST Technical Moderator
Jul 30, 2025 7:02 AM UTC

Hello @PeleAB,

 

Thank you very much for sharing your work!

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Kamurasi-Jordan-Arthur
Associate III
Sep 18, 2025 1:06 PM UTC

Hello Pele AB,
Thanks for sharing, 
I have a few questions though,

Does St modelzoo services really provide a solution of face verification achitectures, like "edgeface, mobilefacenet, ...", Yes I know it has the required backbones but the required lose functions implementations, output shapes and a few other specifics for this scenarios are a bit different.

How exactly did you do this?, Did you have use the yaml file :thinking_face:, or Did you have to custome change the code alitle in the right places?

Am a bit curious.