Skip to main content
AMars.4
Associate III
September 15, 2022
Solved

Project for Nucleo Board with X-NUCLEO-IKA01A1

Hello,

In the annex video it is mentioned that the project archive is available for the Nucleo board project with X-NUCLEO-IKA01A1, however when I download the materials archive it appears to be missing.

Could you confirm this is the case, if so would it be possible to make this project available for download also?

Many thanks,

Anthony

    This topic has been closed for replies.
    Bartosz BORYNA
    Bartosz BORYNABest answer
    ST Employee
    September 16, 2022

    Hi Anthony,

    The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).

    https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8

    Best regards,

    Bartosz

    4 replies

    Bartosz BORYNA
    ST Employee
    September 16, 2022

    Hello Anthony,

    Do you mean NEAI Studio workshop repository on the googledrive ?

    Best regards,

    Bartosz

    AMars.4
    AMars.4Author
    Associate III
    September 16, 2022

    Hi Bartosz,

    This may be what I am looking for, could you share the link?

    Thanks,

    Anthony

    Bartosz BORYNA
    Bartosz BORYNABest answer
    ST Employee
    September 16, 2022

    Hi Anthony,

    The link is below, I've just uploaded the sw example you requested: LAB03_260522.zip , this is Anomaly Detection use case based on current sensor Z-NUCLEO-IKA01A1 and Nucleo-L073, detecting the anomalies of portable USB ventilator (the one used during NEAI WS, reference within the WS slides).

    https://drive.google.com/drive/folders/1KY7U9Ef92gOSMCevfmXQiFQCkdfQ3rg8

    Best regards,

    Bartosz

    AMars.4
    AMars.4Author
    Associate III
    September 16, 2022

    Hi Bartosz,

    That's great, thank you! I will study that.

    Anthony