Skip to main content
Associate II
April 11, 2024
Question

Problems with Cube AI Project

Hello,

I am working on a Human Activity Recognition model with a STMU585CIU6 using Cube AI. In summary, my model takes accelerometer data from my lsm6dsox sensor, and use a frame of 2s of sampling (for ODR 104Hz, it takes 208 samples) as input for the network, which return a prediction among 4 different classes.

After struggling for some time to use the generated functions in my main.c, I managed to perform the inference, but not as I expected. I reached a point where I'm not being able to identify and solve the problem.

I left my board on the desk to run some inferences, and as you can see in the image, the prediction values are the same for all the classes.

LuizF_Ferro_0-1713877492994.png

I would really appreciate if someone could help me to identify what could be possibly wrong. I am mostly suspicious about the network weights/parameters initialization, but I can't really figure it out. Here is an adapted snippet of my main.c:

 

 

 

 

ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
ai_u8 weights[AI_NETWORK_DATA_WEIGHTS_SIZE];
ai_float in_data[AI_NETWORK_IN_1_SIZE];
ai_float out_data[AI_NETWORK_OUT_1_SIZE];

/* AI buffer IO handlers */
ai_buffer *ai_input;
ai_buffer *ai_output;

int main(void) {

 HAL_Init();
 MX_GPIO_Init();
 MX_ICACHE_Init();
 MX_CRC_Init();
 MX_I2C1_Init();
 MX_USART3_UART_Init();

 stmdev_ctx_t dev_ctx;
 uint8_t dummy;
 /* Initialize mems driver interface */
 dev_ctx.write_reg = platform_write;
 dev_ctx.read_reg = platform_read;
 dev_ctx.mdelay = platform_delay;
 dev_ctx.handle = &hi2c1;

 ai_handle network = AI_HANDLE_NULL;
 ai_error err;
 ai_network_report report;

 /** @brief Initialize network */
 const ai_handle acts[] = { activations };
 const ai_handle wgts[] = { weights };
 err = ai_network_create_and_init(&network, acts, wgts);
 if (err.type != AI_ERROR_NONE) {
 printf("ai init_and_create error\n");
 return -1;
 }

 /** @brief {optional} for debug/log purpose */
 if (ai_network_get_report(network, &report) != true) {
 printf("ai get report error\n");
 return -1;
 }

 printf("Model name : %s\r\n", report.model_name);
 printf("Model signature : %s\r\n", report.model_signature);

 ai_input = &report.inputs[0];
 ai_output = &report.outputs[0];
 printf("input[0] : (%d, %d, %d)\r\n", AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_HEIGHT),
 AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_WIDTH),
 AI_BUFFER_SHAPE_ELEM(ai_input, AI_SHAPE_CHANNEL));
 printf("output[0] : (%d, %d, %d)\r\n", AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_HEIGHT),
 AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_WIDTH),
 AI_BUFFER_SHAPE_ELEM(ai_output, AI_SHAPE_CHANNEL));

 int ret = 1;
 ret = lsm6dsox_device_id_get(&dev_ctx, &dummy);

 lsm6dsox_xl_data_rate_set(&dev_ctx, LSM6DSOX_XL_ODR_104Hz);
 lsm6dsox_xl_full_scale_set(&dev_ctx, LSM6DSOX_4g);

 while (1) {
 /* Read accelerometer data */
 lsm6dsox_axis3bit16_t data_raw_acceleration;

 float acceleration_g[3];
 const float sensitivity_a = 0.122f / 1000.0f; // 0.122 mg/LSB converted to g/LSB

 /** @brief Fill input buffer with acceleration/gyroscope values*/
 int bufIdx = 0;
 while (bufIdx < AI_NETWORK_IN_1_SIZE) {
 uint8_t regXL = 0;
 lsm6dsox_xl_flag_data_ready_get(&dev_ctx, &regXL);
 
 if (regXL) {
 lsm6dsox_acceleration_raw_get(&dev_ctx, data_raw_acceleration.i16bit);

 /* int16 -> float conversion */
 acceleration_g[0] = data_raw_acceleration.i16bit[0] * sensitivity_a;
 acceleration_g[1] = data_raw_acceleration.i16bit[1] * sensitivity_a;
 acceleration_g[2] = data_raw_acceleration.i16bit[2] * sensitivity_a;
 
 in_data[bufIdx] = acceleration_g[0];
 in_data[bufIdx + 1] = acceleration_g[1];
 in_data[bufIdx + 2] = acceleration_g[2];
 bufIdx += 3;
 }
 }

 /** @brief Perform inference */
 ai_i32 n_batch;

 /** @brief Set input/output buffer addresses */
 ai_input[0].data = AI_HANDLE_PTR(in_data);
 ai_output[0].data = AI_HANDLE_PTR(out_data);
 ai_input[0].format = AI_BUFFER_FORMAT_FLOAT;
 ai_output[0].format = AI_BUFFER_FORMAT_FLOAT;

 /** @brief Perform the inference */
 n_batch = ai_network_run(network, &ai_input[0], &ai_output[0]);
 if (n_batch != 1) {
 err = ai_network_get_error(network);
 printf("ai run error %d, %d\n", err.type, err.code);
 return -1;
 }

 /** @brief Post-process the output results/predictions */
 printf("Inference output: [");
 float maxValue = -1.0f; // update the highest probability
 int maxIndex = -1;

 /** @brief AI_NETWORK_OUT_1_SIZE = 4 */
 for (int i = 0; i < AI_NETWORK_OUT_1_SIZE; i++) {
 float value;
 value = out_data[i];
 printf("%.2f", value);
 if (i < AI_NETWORK_OUT_1_SIZE - 1) printf(", ");
 if (value > maxValue) {
 maxValue = value;
 maxIndex = i;
 }
 }
 printf("]\r\n");

 // Print activity with highest probability
 const char* activities[AI_NETWORK_OUT_1_SIZE] = {"Sitting", "Stairs", "Standing", "Walking"};
 if (maxIndex != -1) printf("Activity: %s\r\n", activities[maxIndex]);

 }
}

 

 

 

 

I would really appreciate if someone could help me solve this problem. Thanks!

This topic has been closed for replies.

2 replies

fauvarque.daniel
ST Employee
April 23, 2024

Your problem seems to be at least the weights, you should call the ai_network_create_and_init with NULL as the third parameter. The weights are generated automatically by the code generation tool in the file network_data_param.c
 

ai_network_create_and_init(&network, acts, NULL); 

 Here is the pointer to the documentation Documentation/embedded_client_api.html#ref_api_create_init inside the package (normally under ~/STM32Cube/Repository/Pack/STMicroelectronics/X-CUBE-AI/<version>

Regards

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
April 23, 2024

Hi Daniel, thanks for your reply. I had the third parameter set as NULL before, but my problem still persisted. Instead of getting the predicted outputs equal for all classes, using "ai_network_create_and_init(&network, acts, NULL);" gives me an inference output like that:

LuizF_Ferro_0-1713880658864.png

Moving the board or not, the prediction remains dominant for a wrong class.

 

Best regards,

Luiz