Skip to main content
Associate III
Jul 22, 2026 12:54 PM UTC
Solved

Problems running relocatable ai model

hi all,

 

I am trying to flash + run a relocatable / runtime loadable model.

 

The problem is that the inference results are wrong (they never change, no matter what the buffer contains when I start the inference). If I use the stai_model files from the AI Cube Studio, the model works correctly, but is not relocatable…

 

stedgeai.exe generate -m "path/to/model.tflite" --input-data-type uint8 --no-inputs-allocation --no-outputs-allocation --target stm32n6 --st-neural-art --reloc

# final output something like this:

+--------------------------+-------------------------------+------+------------+--------+
| name (addr) | flags | foff | dst | size |
+--------------------------+-------------------------------+------+------------+--------+
| xSPI2 (0x20009332) | 0x02010500 COPY.PARAM.RCACHED | 0 | 0x72000000 | 984321 |
| AXISRAM5 (0x20009338) | 0x03020200 RESET.ACTIV.WRITE | 0 | 0x342e0000 | 409600 |
| AXISRAM4 (0x20009341) | 0x03020200 RESET.ACTIV.WRITE | 0 | 0x34270000 | 196608 |
| <undefined> (0x00000000) | 0x00000000 UNUSED | 0 | 0x00000000 | 0 |
+--------------------------+-------------------------------+------+------------+--------+

 

I try to run the inference as such:


uint32_t ai_run(uint32_t buf) {

LL_ATON_RT_RetValues_t ll_aton_ret;
LL_ATON_RT_Reset_Network(&nn_instance);

LL_ATON_Set_User_Input_Buffer(&nn_instance, 0, buf, BUF_SIZE);
LL_ATON_Cache_MCU_Clean_Invalidate_Range(buf, BUF_SIZE);

do {
ll_aton_ret = LL_ATON_RT_RunEpochBlock(&nn_instance);
/* do NOT wait for event (WFE) as it blocks all other things, potentially corrupting i2c communication.. */
#if 0
if (ll_aton_ret == LL_ATON_RT_WFE) {
LL_ATON_OSAL_WFE();
}
#endif
} while (ll_aton_ret != LL_ATON_RT_DONE);

LL_ATON_Cache_MCU_Invalidate_Range(g_npu_out_buf, g_npu_out_len);
return 0;
}

 

And I try to load the model as follows:


int ai_init(const uintptr_t file_ptr) {

ll_aton_reloc_info rt;
int res;

/* Retrieve the requested RAM size to install the model */
res = ll_aton_reloc_get_info(file_ptr, &rt);

/* Reserve executable memory region to install the model */
uintptr_t exec_ram_addr = (uint32_t)malloc(rt.rt_ram_copy + 0x1f) & ~0x1f;
assert_param(rt.ext_ram_sz == 0);

/* Create and install an instance of the relocatable model */
ll_aton_reloc_config config;
config.exec_ram_addr = exec_ram_addr;
config.exec_ram_size = rt.rt_ram_copy;
config.ext_ram_addr = 0;
config.ext_ram_size = rt.ext_ram_sz;
config.ext_param_addr = NULL;
config.mode = AI_RELOC_RT_LOAD_MODE_COPY; // | AI_RELOC_RT_LOAD_MODE_CLEAR;

res = ll_aton_reloc_install(file_ptr, &config, &nn_instance);
if (res != 0) {
Error_Handler();
}

/* Init the LL ATON stack and the instantiated model */
LL_ATON_RT_RuntimeInit();
LL_ATON_RT_Init_Network(&nn_instance);

LL_Buffer_InfoTypeDef *bufout = ll_aton_reloc_get_output_buffers_info(&nn_instance, 0);

g_npu_out_len = LL_Buffer_len(bufout);
g_npu_out_buf = (uint32_t)malloc(g_npu_out_len + 0x1f) & ~0x1f;
res = ll_aton_reloc_set_output(&nn_instance, 0, g_npu_out_buf, g_npu_out_len);
if (res != 0) {
Error_Handler();
}

assert_param(ll_aton_reloc_is_valid(&nn_instance));

return res;

}

 

does anyone know what I might be doing wrong?

 

best regards, rphii

jean-michel.dBest answer
ST Employee
Jul 28, 2026 4:00 PM UTC

Hi @rphii,

The way to install and initialize the model seems correct. However, I note that LL_ATON_Set_User_Input_Buffer() is used to set the address of the input buffer in the ai_run fct. As for the output, the ll_aton_reloc_set_input() fct should be also used.

Have a good day.

jm

2 replies

Julian E.
ST Technical Moderator
Jul 28, 2026 3:37 PM UTC

Hi ​@rphii,

 

In the Studio, we don’t support it yet.

For the cause in your code, I asked for help, I’ll let you know.

 

If you could maybe attach your model (in zip probably) in the meantime.

 

Have a good day,

Julian.

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jean-michel.dBest answer
ST Employee
Jul 28, 2026 4:00 PM UTC

Hi @rphii,

The way to install and initialize the model seems correct. However, I note that LL_ATON_Set_User_Input_Buffer() is used to set the address of the input buffer in the ai_run fct. As for the output, the ll_aton_reloc_set_input() fct should be also used.

Have a good day.

jm