Skip to main content
ASalc.1
Associate II
Feb 15, 2024 4:46 PM UTC
Question

Problem with LSTM from pytorch.

Hi,

I am trying to deploy a network based on LSTM created with pytorch. The model is analysed correctly but validation on Desktop gives the following error:

 

LOAD ERROR: exception: access violation reading 0x0000000000000004

 

In the MCU a hardfault raises at inference.

I noticed that the error happens because I am accessing the 'hidden_state' of the first LSTM layer to feed it to the second one.

Any ideas about why is this happening?

This is a simple version of the model that reproduces the problem:

 

import torch
from torch import nn

class LSTMModel(nn.Module):
 def __init__(self, input_size, hidden_size, output_size):
 super(LSTMModel, self).__init__()
 self.lstm1 = nn.LSTM(input_size, hidden_size, batch_first=True)
 self.lstm2 = nn.LSTM(hidden_size, hidden_size, batch_first=True)
 self.linear = nn.Linear(hidden_size, output_size)

 def forward(self, x):
 out, (hidden_state, _) = self.lstm1(x)
 out, _ = self.lstm2(hidden_state)
 out = self.linear(out[:, -1, :])
 return out

if __name__ == '__main__':
 model = LSTMModel(14, 8, 14)
 input_data = torch.randn(1, 1, 14)
 _ = model(input_data)

 output_file = 'test-model.onnx'
 model.eval()
 dummy_input = torch.randn(1, 1, 14)
 torch.onnx.export(
 model,
 dummy_input,
 output_file,
 verbose=False)

 

This topic has been closed for replies.

1 reply

fauvarque.daniel
ST Employee
Jul 17, 2024 4:13 PM UTC

Here is an extract of the documentation that explains you how to use stateful LSTM on the target

LSTM

Computes a multi-layer long short-term memory (LSTM) RNN to an input sequence (batch=1, timesteps, features)

  • category: recurrent layer
  • input data types: float32
  • output data types: float32

Specific constraints/recommendations:

  • stateless and stateful (batch=1 only) mode support
  • in stateful mode the user is requested to define two C routines to allocate and deallocate internal layer state.
    • initial state must be provided as part of the allocation routine implementation
    • the two functions to implement are:
      • void _allocate_lstm_states(ai_float **states, ai_u32 size_in_bytes)
      • void _deallocate_lstm_states(ai_float **states)
  • fused activation: gelu, linear, relu, relu_n1_to_1, leaky_relu, relu6, elu, selu, sigmoid, hard_sigmoid, hard_swish, exponential, tanh, softmax, softplus, softsign
  • fused recurrent activation: gelu, linear, relu, relu_n1_to_1, leaky_relu, relu6, elu, selu, sigmoid, hard_sigmoid, hard_swish, exponential, tanh, softmax, softplus, softsign
  • return_state not supported
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.