Skip to main content
rickforescue
Associate II
March 15, 2022
Question

no source available for "ai_platform_inputs_get()" X-cube.AI version 7.1.0 I attach a basic code snippet which might be helpful in recreating the problem

/* USER CODE BEGIN PV */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
/* USER CODE END PV */
 
int main(void){
...
	// Chunk of memory used to hold the intermediate values for neural network
	AI_ALIGNED(32) ai_u32 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
 
	// Buffers used to store input and output tensors
	AI_ALIGNED(32) ai_i32 in_data[AI_NETWORK_IN_1_SIZE_BYTES];
	AI_ALIGNED(32) ai_i32 out_data[AI_NETWORK_OUT_1_SIZE_BYTES];
 
	// Pointer to our model
	ai_handle my_model = AI_HANDLE_NULL;
 
	// structs that point to our input and output data and some meta data
	ai_input = ai_network_inputs_get(my_model , NULL);
	ai_output = ai_network_outputs_get(my_model , NULL);
 
....
}

As seen the function ai_network_inputs_get(ai_handle network, ai_u16 *n_buffer) resides in the network.c file and it makes a call to the ai_platform_inputs_get(network, n_buffer); in file ai_platform_interface.h

It doesnt give me any errors while running but the code breaks while getting the ai_buffer to the input of the model

I dont know what possibly can go wrong. Should I explicitally implement these functions in main() ? There exists some literature and videos on web but they are old.

Is there anyone who has faced similar problems or knows solutioon to this?

Thanks in advance

This topic has been closed for replies.

1 reply

rickforescue
Associate II
March 16, 2022

Alright, I think I found the solution to the problem.

The problem is before calling the ai_network_inputs_get function the ai model has to be created.

So the solution looks like this

 /* USER CODE BEGIN PV */
 static ai_buffer *ai_input;
 static ai_buffer *ai_output;
 /* USER CODE END PV */
 
 int main(void){
 ...
 	// Chunk of memory used to hold the intermediate values for neural network
 	AI_ALIGNED(32) ai_u32 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
 
 	// Buffers used to store input and output tensors
 	AI_ALIGNED(32) ai_i32 in_data[AI_NETWORK_IN_1_SIZE_BYTES];
 	AI_ALIGNED(32) ai_i32 out_data[AI_NETWORK_OUT_1_SIZE_BYTES];
 
 	// Pointer to our model
 	ai_handle my_model = AI_HANDLE_NULL;
 ..........
 /* USER CODE BEGIN 2 */
 ..........
 ai_network_params ai_params =
 {
		 {
				AI_NETWORK_DATA_WEIGHTS(ai_network_data_weights_get()),
				AI_NETWORK_DATA_ACTIVATIONS(activations)
		 }
 };
 
 // Create instance of the neural network
 ai_err = ai_network_create(&my_model, AI_NETWORK_DATA_CONFIG);
 if (ai_err.type != AI_ERROR_NONE)
 {
	 buf_len = sprintf(buf, "Error: Could not create NN instance\r\n");
	 HAL_UART_Transmit(&huart3, (uint8_t *)buf, buf_len, 100);
	 while(1);
 }
 
 // Initialize neural network. At this point we are ready to make inferences
 if (!ai_network_init(my_model, &ai_params))
 {
	 buf_len = sprintf(buf, "Error: could not initialize NN\r\n");
	 HAL_UART_Transmit(&huart3, (uint8_t *)buf, buf_len, 100);
	 while(1);
 }
 
 // structs that point to our input and output data and some meta data 
 	ai_input = ai_network_inputs_get(my_model, NULL);
 	ai_output = ai_network_outputs_get(my_model, NULL);
 
 ....
 }