Associate III
January 11, 2024
Question
NanoEdgeAI Studio - Proper Signal Formatting?
- 7 replies
- 5306 views
Hi STM Community-
Context: X-Nucleo-53L8A1 / Nucleo-L476RG
16 zones per line of distance measurements are being captured by NanoEdgeAI in an attempt to generate an anomaly detection AI model. 16 axes correlate to 16 measurement zones. Measurements are in mm. The data seems to be properly formatted; however, when the "Signal" is added, NanoEdgeAI indicates there are not sufficient values for FFT to be performed. MIN, MAX, & MEANS are calculated.
Files attached. Pls advise.
Thanks in advance,
Kelly