Skip to main content
Associate II
Apr 23, 2025 7:06 AM UTC
Solved

NanoEdge build error: RTOS\RTOS.axf: Error: L6200E: Symbol _fminf is multiply defined

I would like to ask how NanoEdge AI embeds multiple library models in one code, for example: I compiled a project called "test" in the Keil compiler and I want to create a project similar to an official demo video. Under the same project, there is both an anomaly detection (AD) library for learning and a multi classification (N-Classfial) library for classifying abnormal situations.

Now, I have trained two models for these two libraries, but the problem is that I don't know how to embed these two models into the same project for use. I am using the v5.0.2 version of NanoEdge AI STUDIO.

Can you help me solve this problem? Thank you.

Julian E.
Julian E.Best answer
ST Technical Moderator
Apr 23, 2025 10:01 AM UTC

Hello @szxx,

 

In the last step of NanoEdge AI Studio, the compilation, you can select the Multi-library option. 

You need to enter a name to your library that will be used as a suffix for the files to include in your project and in the function names, for you to freely use each library.

 

For example, here is a classification project, where I call my library lib1:

JulianE_1-1745401183902.png

Here is the zip that you get:

JulianE_2-1745401208693.png

You can see that my knowledge, libneai and NanoEdgeAI files all have the suffix lib1.

 

We can also look at the function in the header file NanoedgeAI_lib1.h:

	/**
	 * @brief Initialization must be called at the beginning to load the knowledge. 
	 * This buffer is defined in the header file knowledge.h provided in the .zip file
	 * @retval NEAI_OK in case of success.
	 */
	enum neai_state neai_classification_init_lib1(const float knowledge_buffer[]);

	/**
	 * @brief This function returns the class identified
	 * @param data_input[] [IN]: Signal to be classified AXIS_NUMBER * DATA_INPUT_USER
	 * @param output_buffer[] [OUT]: Contains the probabilities for all classes
	 * @param *id_class [OUT]: Variable that contains the class ID with the highest probabilities
	 * @retval NEAI_OK in case of success.
	 */
	enum neai_state neai_classification_lib1(float data_input[], float output_buffer[], uint16_t *id_class);

 

As you can see my functions also have the suffix lib1.

 

Now if you want to add another library, you will have to select multilibrary and set a name, like lib2.

 

Let's say, you have a classification library called lib1 and an anomaly detection called lib2. In your project, you need to:

  1. Include everything
  2. Initialise both libraries (for anomaly detection you either use a knowledge or retrain the library, or both)
  3. use the anomaly detection learn function to retrain (optional)
  4. Fill a buffer of data
  5. Do anomaly detection
  6. Do classification if similarity is low (if anomaly detection detected an anomaly)

 

For example, something like this:

#include "NanoEdgeAI_lib1.h"
#include "NanoEdgeAI_lib2.h"
#include "knowledge_lib1.h"
#include "knowledge_lib2.h"


int main(void) {
 // Initialize models
 neai_state1 = neai_classification_init_lib1(knowledge_buffer);
 neai_state2 = neai_anomalydetection_knowledge_lib2(knowledge_buffer);

 if (neai_state1 == NEAI_OK and neai_state2 == NEAI_OK ) {
 while (1) {
 // Fill data_inputwith sensor data here

 // Run Anomaly Detection
 neai_anomalydetection_detect_lib2(float data_input[], uint8_t *similarity);

 // If similarity is low, most likely an anomaly
 if (similarity <= 90) {
 neai_classification_lib1(float input_buffer[], float output_buffer[], uint16_t *id_class);
 }
 // Do something with the results
 }
 }
 //else error in init
}

 

 

Documentation about libraries function:

Anomaly detection:  https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_anomaly_detection_(AD)

Classification: https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_n-class_classification_(nCC) 

 

You can also find code example here:

stm32ai-nanoedge-datalogger/Drivers at main · stm32-hotspot/stm32ai-nanoedge-datalogger

These code are the datalogger generator source code. These code both include datalogging and using a library so you can take a look.

(be careful to use the command in the readme to clone the repository as it needs external ressources)

 

have a good day,

Julian

 

 

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

9 replies

Julian E.
Julian E.Best answer
ST Technical Moderator
Apr 23, 2025 10:01 AM UTC

Hello @szxx,

 

In the last step of NanoEdge AI Studio, the compilation, you can select the Multi-library option. 

You need to enter a name to your library that will be used as a suffix for the files to include in your project and in the function names, for you to freely use each library.

 

For example, here is a classification project, where I call my library lib1:

JulianE_1-1745401183902.png

Here is the zip that you get:

JulianE_2-1745401208693.png

You can see that my knowledge, libneai and NanoEdgeAI files all have the suffix lib1.

 

We can also look at the function in the header file NanoedgeAI_lib1.h:

	/**
	 * @brief Initialization must be called at the beginning to load the knowledge. 
	 * This buffer is defined in the header file knowledge.h provided in the .zip file
	 * @retval NEAI_OK in case of success.
	 */
	enum neai_state neai_classification_init_lib1(const float knowledge_buffer[]);

	/**
	 * @brief This function returns the class identified
	 * @param data_input[] [IN]: Signal to be classified AXIS_NUMBER * DATA_INPUT_USER
	 * @param output_buffer[] [OUT]: Contains the probabilities for all classes
	 * @param *id_class [OUT]: Variable that contains the class ID with the highest probabilities
	 * @retval NEAI_OK in case of success.
	 */
	enum neai_state neai_classification_lib1(float data_input[], float output_buffer[], uint16_t *id_class);

 

As you can see my functions also have the suffix lib1.

 

Now if you want to add another library, you will have to select multilibrary and set a name, like lib2.

 

Let's say, you have a classification library called lib1 and an anomaly detection called lib2. In your project, you need to:

  1. Include everything
  2. Initialise both libraries (for anomaly detection you either use a knowledge or retrain the library, or both)
  3. use the anomaly detection learn function to retrain (optional)
  4. Fill a buffer of data
  5. Do anomaly detection
  6. Do classification if similarity is low (if anomaly detection detected an anomaly)

 

For example, something like this:

#include "NanoEdgeAI_lib1.h"
#include "NanoEdgeAI_lib2.h"
#include "knowledge_lib1.h"
#include "knowledge_lib2.h"


int main(void) {
 // Initialize models
 neai_state1 = neai_classification_init_lib1(knowledge_buffer);
 neai_state2 = neai_anomalydetection_knowledge_lib2(knowledge_buffer);

 if (neai_state1 == NEAI_OK and neai_state2 == NEAI_OK ) {
 while (1) {
 // Fill data_inputwith sensor data here

 // Run Anomaly Detection
 neai_anomalydetection_detect_lib2(float data_input[], uint8_t *similarity);

 // If similarity is low, most likely an anomaly
 if (similarity <= 90) {
 neai_classification_lib1(float input_buffer[], float output_buffer[], uint16_t *id_class);
 }
 // Do something with the results
 }
 }
 //else error in init
}

 

 

Documentation about libraries function:

Anomaly detection:  https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_anomaly_detection_(AD)

Classification: https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Library_for_n-class_classification_(nCC) 

 

You can also find code example here:

stm32ai-nanoedge-datalogger/Drivers at main · stm32-hotspot/stm32ai-nanoedge-datalogger

These code are the datalogger generator source code. These code both include datalogging and using a library so you can take a look.

(be careful to use the command in the readme to clone the repository as it needs external ressources)

 

have a good day,

Julian

 

 

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
szxxAuthor
Associate II
Apr 23, 2025 10:12 AM UTC

To @Julian E. :

Thank you very much for helping me solve the problem of how to embed two libraries in the same project. However, after embedding the two libraries, I encountered this problem:

RTOS\RTOS.axf: Error: L6200E: Symbol _fminf multiply defined (by NanoEdgeAI_yuan.o and NanoEdgeAI_san.o).

I don't know how it was caused. Could you help me solve it again? Thank you very much!
Wish you a good mood every day.

szxx

 

Julian E.
ST Technical Moderator
Apr 23, 2025 1:03 PM UTC

Hello @szxx,

 

Indeed, it seems that there is a bug with keil.

Because of another bug, from Arm this time, we have to make a simple test _fminf to warn the user if he is using keil.

 

We will solve it in the next version, but until then, can you test the following:

 

if you check the symbols in each:

nm NanoEdgeAI_san.o | grep fminf
nm NanoEdgeAI_yuan.o | grep fminf

You’ll see _fminf is defined in both.

 

Then to avoid clashing, rename symbols in just one object file (say the classification one):

objcopy --redefine-sym _fminf=_fminf_san NanoEdgeAI_san.o

 

Rebuild a new .a file with the fixed object

ar rcs libneai_san_fixed.a NanoEdgeAI_san.o


In Keil:

  • Link both libneai_yuan.a and libneai_san_fixed.a
  • Your symbol clash is gone.
  • Use their functions as usual.

 

Sorry for the inconvenience.

Because of this, you will have to do it each time you want to deploy a new library.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HSpre.1
Associate II
Feb 11, 2026 9:24 AM UTC

Hi all , in the latest version 5.1 of Nanoedge AI I cannot find the Multi-library option anymore. How do i go about doing this with version 5.1?

Visitor II
Feb 12, 2026 7:30 AM UTC

I have the same problem. In previous versions I used to multilibrary but now missing. It's frustrating. I need to finish a big project and now this issue. Anybody know if will be fixed in next version?

Julian E.
ST Technical Moderator
Feb 12, 2026 9:34 AM UTC

Hi @HSpre.1, @prtaboss,

 

Sorry for this issue. Multi library is not an option in 5.1.

 

I am discussing internally to know if they plan to add it back in the next NanoEdge release.

My understanding is that this is indeed planned.

 

I will contact you in private to find a solution in the meantime.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
HSpre.1
Associate II
Feb 12, 2026 12:32 PM UTC

I am still in the process of testing. But I think i have a stopgap solution (can't wait) 

 

I export the .a and .h file into a folder named for example "MODEL1" and then I put a .bat file in the same folder:

 

The bat file renames everything acoording to folder name. I then put the renamed library and h file in stm32cubeide

functions

variables

filenames

it also updates the Defines in .h files.

 

Currently it is compiling. my 2 classification models ,still need to test further...

Might help someone

 

 

==========================================================

@Echo off
setlocal enabledelayedexpansion

:: 1. Find Toolchain
set "CUBE_ROOT=C:\ST\STM32CubeIDE_*"
for /d %%D in (%CUBE_ROOT%) do (
for /d %%P in ("%%D\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.*") do (
set "TOOLCHAIN_PATH=%%P\tools\bin"
)
)

if not exist "!TOOLCHAIN_PATH!\arm-none-eabi-nm.exe" (
echo [ERROR] Toolchain not found.
pause & exit /b
)

set "NM=!TOOLCHAIN_PATH!\arm-none-eabi-nm.exe"
set "OBJCOPY=!TOOLCHAIN_PATH!\arm-none-eabi-objcopy.exe"
for %%I in (.) do set "PREFIX=%%~nxI"

set LIB_NAME=libneai.a
set HEADER_NAME=NanoEdgeAI.h

:: 2. Process Library
echo [INFO] Extracting and renaming library symbols...
"%NM%" %LIB_NAME% --defined-only | findstr " T " > symbols_raw.txt
if exist symbols_rename.txt del symbols_rename.txt
for /f "tokens=3" %%A in (symbols_raw.txt) do (echo %%A %PREFIX%_%%A >> symbols_rename.txt)
"%OBJCOPY%" --redefine-syms=symbols_rename.txt %LIB_NAME% lib%PREFIX%.a

:: 3. Process Header (Using word boundaries \b to avoid mangling)
echo [INFO] Deep-renaming Header and Guards for %PREFIX%...
powershell -Command ^
"$content = Get-Content '%HEADER_NAME%';" ^
"$content = $content -replace '#ifndef NANOEDGEAI_H', '#ifndef %PREFIX%_NANOEDGEAI_H';" ^
"$content = $content -replace '#define NANOEDGEAI_H', '#define %PREFIX%_NANOEDGEAI_H';" ^
"$content = $content -replace '\binput_signal\b', '%PREFIX%_input_signal';" ^
"$content = $content -replace '\bid_class\b', '%PREFIX%_id_class';" ^
"$content = $content -replace '\bprobabilities\b', '%PREFIX%_probabilities';" ^
"$content = $content -replace '\bstate\b', '%PREFIX%_state';" ^
"$content = $content -creplace 'neai_', '%PREFIX%_neai_';" ^
"$content = $content -creplace 'NEAI_', '%PREFIX%_NEAI_';" ^
"$content | Set-Content '%PREFIX%_%HEADER_NAME%'"

:: 4. INTEGRATED VERIFICATION CHECK
echo [INFO] Verifying changes in lib%PREFIX%.a...
"%NM%" lib%PREFIX%.a | findstr /C:" %PREFIX%_neai_classification_init" > nul
if %errorlevel% equ 0 (
echo [SUCCESS] Library verified: Symbols renamed to '%PREFIX%_neai_'.
) else (
echo [ERROR] Verification FAILED: Renamed symbols not found in lib%PREFIX%.a.
)

del symbols_raw.txt & del symbols_rename.txt
pause

Julian E.
ST Technical Moderator
Feb 24, 2026 9:49 AM UTC

Hi,

 

We are going to support it in the next major release.

In the meantime, please look at this workaround:

NanoEdge AI Studio 5.1.0 multi library - STMicroelectronics Community

 
 
Have a good day,
Julian
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.