NanoEdge AI Studio Not Receiving Data from STWINBX1 Despite Correct Configuration
- 14 replies
- 4129 views
Hi everyone,
I’m currently working on a project involving predictive maintenance and anomaly detection using the STWINBX1 (STEVAL-STWINBX1) board. I’ve successfully configured the board and flashed it using STM32CubeIDE, ensuring everything is set up as expected. I’ve also downloaded the NanoEdge Datalogger and flashed it using STM32 ST-Link Utility, but despite everything being correctly configured, NanoEdge AI Studio is not receiving any data from the board.
Here’s what I’ve checked so far:
- The board is properly connected to my PC.
- I’ve verified the COM port number, and I'm sure it's correct.
- The NanoEdge Datalogger has been flashed successfully.
- The board’s sensors are properly connected and powered.
Despite these steps, the data is not being received in NanoEdge AI Studio. I’ve also ensured that no other processes are using the COM port, and I’ve checked that all configurations are aligned with the expected setup.
Can anyone suggest what could be causing this issue or guide me on where I might be going wrong? I need to collect data for training my model, and this issue is blocking my progress.
Thanks in advance!