Skip to main content
Associate II
Mar 30, 2026 6:55 PM UTC
Solved

n6-dk hard fault with unresponsive debugger

I have been playing with the n6-dk for a while and today something unexpected happened.

When I try to run the stock code provided in the model zoo services, the board flashes for a moment at startup and the debugger and the board become unresponsive (requiring power cycling).

Another weird thing is that if I flash the code and connect the board to a power source the code seems to be running correctly. I tried with another desktop experiencing the same issue. I also tried to do a mass erase and fresh flashing of fsbl, source, and network code.

This was not a problem before, for weeks I run the code with the board connected to my desktop, I have never seen the code crash like that (normally, if something in the code is wrong, I hit a fault and the board get stuck in a sig handler loop).

Has anyone experienced anything similar?

FBLBest answer
ST Technical Moderator
Apr 3, 2026 4:03 PM UTC

Hello @rfronteddu 

Did you follow this article How to run AI models from model zoo on STM32N6

If so, to narrow it down, I suggest you to check basic debugging: Flash a simple example to blink led.

Then, try to debug this project:

  • If it debugs correctly, the basic ST‑LINK and board are OK, and the problem is specific to the Model Zoo application or maybe memory layout.
  • If this simple example also fails, you should focus on ST‑LINK firmware, cable, option bytes, or the board itself.

You need to reproduce the issue with minimum firmware.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

2 replies

FBLBest answer
ST Technical Moderator
Apr 3, 2026 4:03 PM UTC

Hello @rfronteddu 

Did you follow this article How to run AI models from model zoo on STM32N6

If so, to narrow it down, I suggest you to check basic debugging: Flash a simple example to blink led.

Then, try to debug this project:

  • If it debugs correctly, the basic ST‑LINK and board are OK, and the problem is specific to the Model Zoo application or maybe memory layout.
  • If this simple example also fails, you should focus on ST‑LINK firmware, cable, option bytes, or the board itself.

You need to reproduce the issue with minimum firmware.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
Apr 3, 2026 4:18 PM UTC

II have followed the article and successfully deployed the base and modified code. For my tests, I reverted back to the stock code doing a mass erase.

I am waiting for my other discovery kit to come back to validate if it's a problem with the board or with something else that changed. I noticed that at the same time this problem happened CUBE IDE updated the ST-LINK drivers.

It's very peculiar to me that I have never seen the board become unresponsive (i.e. disconnecting me from the debugger, normally if I did something wrong a fault would be triggered and the board would get stuck in one of the fault handlers of the code.