Skip to main content
Visitor II
Nov 17, 2026 10:21 AM UTC
Question

N6 CubeAI Studio vs Edge AI Cloud benchmarking on ssd_mobilenetv1_pt_voc_300_qdq_int8.onnx

Hi,
I’m benchmarking this object detection model from modelzoo: ssd_mobilenetv1_pt_voc_300_qdq_int8.onnx (https://github.com/STMicroelectronics/stm32ai-modelzoo/blob/main/object_detection/ssd_mobilenetv1_pt/Public_pretrainedmodel_public_dataset/voc/ssd_mobilenetv1_pt_voc_300/ssd_mobilenetv1_pt_voc_300_qdq_int8.onnx)
I managed to reproduce the intended 41ms inference duration on STM32N6570-DK using ST Edge AI Developer Cloud. 
I also tried to reproduced this test offline with CubeAI  (Edge AI core 4.1) and a STM32N6 Nucleo board but didn’t get better than 116ms.
The DK is in overdrive mode by default and the Nucleo is not. But this shouldn’t explain this huge difference (?)
I tried several optimisation parameters as well as the --use-onnx-simplifier option. Also memory mapping looks similar in both case.
Does any one have an idea ?

Thanks

Mathieu

1 reply

hamitiya
ST Technical Moderator
Nov 17, 2026 12:37 PM UTC

Hello ​@Mathieu C 

Do you have logs for both execution?

 

It could be parameters for ST Neural-ART Accelerator, including with no exception, `--optimization 3` or `--enable-epoch-controller`

 

Best regards,

Yanis

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.