Skip to main content
Associate II
Feb 28, 2025 2:56 PM UTC
Solved

Issue with TensorFlow Dense Layer Conversion to .nb Format

Hello,

I am encountering an issue when converting a TensorFlow Dense layer to .tflite and subsequently using the ST Edge AI tool to convert it to .nb format, following the ST Edge AI Guide for MPU.

When using a lower-dimensional input, the conversion succeeds. For example, the following code works as expected:

 

input_features = tf.keras.Input(shape=(1, 384), dtype=tf.float32)

output = tf.keras.layers.Dense(1536)(input_features)

model = tf.keras.Model(inputs=input_features, outputs=output)

 

However, increasing the input dimension to (1500, 384) results in the following error:

 

ST Edge AI Core v2.0.0-20049

PASS: 0%| | 0/2 [00:00<?, ?it/s]

Galcore warning: MMU is disabled!

E [main.c:vnn_VerifyGraph:93]CHECK STATUS(-3:The requested set of parameters produce a configuration that cannot be supported.)

E [main.c:main:236]CHECK STATUS(-3:The requested set of parameters produce a configuration that cannot be supported.)

E 21:37:15 Fatal model generation error: 64768

E010(InvalidModelError): Error during NBG compilation, model is not supported

 

Is there a known limitation on the input/output dimensions for Dense layers when converting to .nb format? If so, is there a recommended approach to handle larger dimensions, or any workarounds to enable successful conversion and NPU acceleration?

Thank you for your time and assistance.

Best regards,
Justin

This topic has been closed for replies.
Julian E.
Julian E.Best answer
ST Technical Moderator
Mar 3, 2025 10:35 AM UTC

Hello @J-WTY ,

 

You can find the constraint regarding the ST Edge AI Core here: https://stedgeai-dc.st.com/assets/embedded-docs/index.html

Depending on what you use, meaning tensorflow, tflite, keras or onnx and if you use the NPU (example: STM32N6), the constraint on the layers may be different. You can find a dedicated page for each one of them.

 

There is a commun constraint that is this one: 

Common constraints

  • input and output tensors must be not dynamic.
    • variable-length batch dimension (i.e. (None,)) is considered as equal to 1
    • must not be greater than 6D
    • dimension must be in the range [0, 65536[
    • batch dimension is not supported for the axis parameter
  • data type for the weights/activations tensors must be:
    • float32, int8, uint8
    • only int32 for the bias tensor is considered
    • for some operators, bool type is also supported
  • operator with un-connected output is not supported
  • mixed data operations (i.e hybrid operator) are not supported, activations and weights should be quantized
  • generated c-model is always channel-last (or NHWC format)
  • 1D operator is mapped on the respective 2D operator by adding a singleton dimension on the input: (12,3) -> (12, 0, 3)

 

So, instead of using a (1500,384) shape, please use a (1,1500,384) shape. For example:

input_features = tf.keras.Input(shape=(1, 1500, 384), dtype=tf.float32)
output = tf.keras.layers.Dense(1536)(input_features)
model = tf.keras.Model(inputs=input_features, outputs=output)

Have a good day,
Julian
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

5 replies

Julian E.
Julian E.Best answer
ST Technical Moderator
Mar 3, 2025 10:35 AM UTC

Hello @J-WTY ,

 

You can find the constraint regarding the ST Edge AI Core here: https://stedgeai-dc.st.com/assets/embedded-docs/index.html

Depending on what you use, meaning tensorflow, tflite, keras or onnx and if you use the NPU (example: STM32N6), the constraint on the layers may be different. You can find a dedicated page for each one of them.

 

There is a commun constraint that is this one: 

Common constraints

  • input and output tensors must be not dynamic.
    • variable-length batch dimension (i.e. (None,)) is considered as equal to 1
    • must not be greater than 6D
    • dimension must be in the range [0, 65536[
    • batch dimension is not supported for the axis parameter
  • data type for the weights/activations tensors must be:
    • float32, int8, uint8
    • only int32 for the bias tensor is considered
    • for some operators, bool type is also supported
  • operator with un-connected output is not supported
  • mixed data operations (i.e hybrid operator) are not supported, activations and weights should be quantized
  • generated c-model is always channel-last (or NHWC format)
  • 1D operator is mapped on the respective 2D operator by adding a singleton dimension on the input: (12,3) -> (12, 0, 3)

 

So, instead of using a (1500,384) shape, please use a (1,1500,384) shape. For example:

input_features = tf.keras.Input(shape=(1, 1500, 384), dtype=tf.float32)
output = tf.keras.layers.Dense(1536)(input_features)
model = tf.keras.Model(inputs=input_features, outputs=output)

Have a good day,
Julian
​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
J-WTYAuthor
Associate II
Mar 24, 2025 1:09 AM UTC

Hello @Julian E.

I found it work to use (1, 1500, 384) for the shape of Input layer!

Thanks for your help a lot!

But I want to know that is this due to the constraint "1D operator is mapped on the respective 2D operator by adding a singleton dimension on the input: (12,3) -> (12, 0, 3)"? Thanks!

 

Best regards,

J-WTY

 

Julian E.
ST Technical Moderator
Mar 24, 2025 2:00 PM UTC

Hello @J-WTY,

 

Thanks for the update!

 

Regarding your question, I am not exactly sure.

In my opinion, because ST Edge AI core was originally made for images, they probably already had 2D operators in C code.

So instead of developing the 1D variant for each operator, they mapped your 1D input to 2D as it is probably the same thing either way.

 

Keep in mind that I am speculating here, but I think it is a reasonable explanation.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
J-WTYAuthor
Associate II
Mar 18, 2025 4:09 PM UTC

Hello Julian E.,

Thanks for your answer, I'm sorry for ignoring your reply for days.

with the help of your suggestion, I will try to solve it as soon as possible, thanks!

 

Best regards,

J-WTY