Issue with 16-bit input and 16-bit weight convolution on STM32N6 ConvAcc
- 3 replies
- 817 views
Hi all,
According to the STM32N6 reference manual (see attached figure), both the diagram and the text description state that the ConvAcc should support 16-bit input × 16-bit weight (16×16) operations.

To verify this, I designed a simple test model(see attached files):
Input: 4×4 tensor (all ones)
Kernel: 3×3 (all ones)
Expected output: 2×2 tensor
When I set the SIMD field to 1, the ConvAcc performs 8-bit input × 8-bit weight (8×8) operations, and the output results are correct as expected.
When I set the SIMD field to 2, the ConvAcc performs 16-bit input × 8-bit weight (16×8) operations, and the results are also correct.
My questions are:
Does the ConvAcc really support 16×16 convolution (16-bit input × 16-bit weight) as described in the reference manual?
If yes, how should I correctly configure the fields of LL_Convacc_InitTypeDef to enable 16×16 operation? (e.g., simd, inbytes_f, outbytes_o, kseten, etc.)