Skip to main content
Kamurasi-Jordan-Arthur
Associate III
Aug 11, 2026 7:58 AM UTC
Question

In consistence btw generated model files and CLI command parameter

Dear ST Edge AI Support Team,

We are deploying a YOLO11n person-detection model on the STM32N6 NPU using the relocatable
(LRUN) generation flow. While decoding the generated runtime buffer descriptors on-target, we
found that the top-level *input* user-IO buffer's channel-position metadata disagrees with its
own reported memory shape, and does not change when explicitly requesting a channel-last input
layout.

Configuration

 Target: STM32N6
 ST Edge AI Core v4.0.1-20581 7ed50de05
 Model: yolo11n_256_quant_pc_uf_od_coco-person-st.tflite (quantized, uint8 input, 256x256x3)
 stedgeai cli command (as echoed by network_generate_report.txt):
   "stedgeai generate --model yolo11n_256_quant_pc_uf_od_coco-person-st.tflite --relocatable
    split --target stm32n6 --no-inputs-allocation --no-outputs-allocation --optimization
    balanced --st-neural-art user_profile@profile-neural-art.json --name network --verbosity 1
    --c-api st-ai --inputs-ch-position chlast --workspace ./workspace --output ./outputs"

Issue

 The generated network_generate_report.txt confirms `--inputs-ch-position chlast` was received
 and correctly resolved at the IR level - the layer table shows the model input as
 `[b:1,h:256,w:256,c:3]` (line 9), i.e. NHWC as requested.

 However, the generated runtime buffer descriptor for the same input tensor is
 self-contradictory, and this is unchanged whether or not `--inputs-ch-position chlast` is
 passed:

 In outputs/network.c, LL_ATON_Input_Buffers_Info_network():

   static const uint32_t buff_info__mem_shape_F_1_256_256_3[] = { 1, 256, 256, 3 };
   ...
   .mem_shape = buff_info__mem_shape_F_1_256_256_3,
   .mem_ndims = 4,
   .chpos     = CHPos_First,   /* <- inconsistent with mem_shape below */

 Per ll_aton_NN_interface.h, `chpos` is documented as "Position of channels dimension in mem
 shape". `mem_shape = {1, 256, 256, 3}` unambiguously has the channel dimension (3) at index 3
 (last), matching the buffer's own byte size (196608 = 256*256*3*1 byte) and the IR table above.
 A `chpos` of `CHPos_First` implies the channel dimension is at index 1 (value 256), which is
 wrong on its face.

 The same contradiction appears independently in outputs/network_c_info.json, buffer
 "Input_5_out_0":

   "shape": [1, 256, 256, 3],
   "channel_first": true,
   "channel_last": false,

 i.e. the shape field is NHWC while channel_first/channel_last flags say the opposite.

 For comparison, the *output* buffer's equivalent fields are internally consistent
 (mem_shape={1,5,1344}, chpos=CHPos_First, with the channel-like dim of 5 genuinely at index 1),
 so this appears isolated to the top-level *input* user-IO buffer under this particular
 combination of options.

What we have tried

 Regenerated the model from scratch with `--inputs-ch-position chlast` added - the IR-level
 shape resolves correctly (see report line 9), but the emitted chpos/channel_first value for the
 input buffer descriptor in network.c and network_c_info.json does not change.
 Cross-checked byte size (196608 bytes = 256*256*3) and camera pipeline layout (DCMIPP/ISP always
 hands frames over as interleaved NHWC) against both mem_shape and shape - both agree with NHWC,
 only chpos/channel_first disagree.
 Worked around this on our side by no longer branching on chpos/channel_first for the input
 buffer and instead reading mem_shape directly, with a byte-size sanity check
 (H*W*C*bytes_per_element == buffer length) as a guard against a genuine future layout change.

Request

 Can you confirm whether chpos/channel_first for the top-level input buffer is expected to
 reflect the buffer's own mem_shape/shape (as documented), or whether there is a known
 discrepancy for `--relocatable split --no-inputs-allocation --c-api st-ai` output?
 Is `--inputs-ch-position chlast` expected to affect this specific generated field, or only the
 model's internal/IR-level layout?
 Is there a more authoritative field or API (rather than chpos/channel_first) we should use at
 runtime to determine the true memory layout of a `LL_Buffer_InfoTypeDef` user-IO buffer?

Attachments

 model_files/outputs/network_generate_report.txt (generation log, includes CLI args and IR
 layer table)
 model_files/outputs/network.c (LL_ATON_Input_Buffers_Info_network / LL_ATON_Output_Buffers_Info_network)
 model_files/outputs/network_c_info.json (buffers[] entries for Input_5_out_0 / Transpose_1177_out_0)