Skip to main content
ICopp
Visitor II
November 7, 2019
Question

I am trying to import on CUBE AI the HAR model used in the official tutorial. I repeatedly got the following error at the end of "Validate on Desktop": TOOL ERROR: Weights are incompatible with model: 794136 loaded, 89864 found Any tips please?

This is the log of Validation on Desktop

Starting AI validation on desktop with random data...

  

Neural Network Tools for STM32 v1.1.0 (AI tools v4.1.0) 

-- Importing model 

-- Importing model - done (elapsed time 1.366s) 

-- Building X86 C-model 

. 

-- Building X86 C-model - done (elapsed time 35.235s) 

-- Setting inputs (and outputs) data 

Using random input, shape=(10, 270) 

-- Running X86 C-model 

TOOL ERROR: Weights are incompatible with model: 794136 loaded, 89864 found 

Creating report file C:\Users\Ilario Coppola\.stm32cubemx\stm32ai_output\network_validate_report.txt 

TOOL ERROR: Weights are incompatible with model: 794136 loaded, 89864 found 

Using TensorFlow backend. 

TOOL ERROR: Weights are incompatible with model: 794136 loaded, 89864 found

    This topic has been closed for replies.