Skip to main content
RBenf.11
Visitor II
February 12, 2022
Question

https://wiki.st.com/stm32mcu/wiki/AI:How_to_perform_motion_sensing_on_STM32L4_IoTnode I'm using X-CUBE_AI 7.1.0 but having trouble compiling this example project for motion detection.

ai_input[0].n_batches = 1;

'ai_buffer' {aka 'struct ai_buffer_'} has no member named 'n_batches'

network.h

AI_DEPRECATED

#define AI_NETWORK_IN \

 ai_network_inputs_get(AI_HANDLE_NULL, NULL)

This comes up invalid initializer error.

Any ideas? The initial code compiled ok with the acc data apart from a bug in cubemx where the lsm6dsl.h could not be found.

This topic has been closed for replies.

5 replies

Umahe.1
Associate II
June 15, 2022

I got the similar error as I were using the reference code from 7.0.0 and found that with upgradation of Software pack from 7.0.0 to 7.1.0. There is a new way of assigning the input and getting the output. You can check that if that's the mistake if you're doing too.

AC.7
Associate
July 9, 2022

Any answer for this question? I'm facing the same issue

KK.10
Visitor II
February 28, 2023

See my answer below.

KK.10
Visitor II
February 28, 2023

X-CUBE-AI 7.0 code example doesn't work with later versions. In my case 7.3.0.

Completely disregard example code for 7.0 version and use code from ST example: "How to perform motion sensing on STM32L4 IoTnode".

Section 6: "Create an STM32Cube.AI application using X-CUBE-AI".

mpark.21
Visitor II
March 2, 2023

thanks you