Skip to main content
Associate III
Feb 17, 2025 11:27 AM UTC
Solved

How to use STEVAL-C34KAT2 with STEVAL-STWINBX1 ?

I am using the STEVAL-C34KAT2 with the STEVAL-STWINBX1 which is running the software FP-SNSDATALOG2 V3.0.0.

Do I need to change anything in the FP-SNSDATALOG2 V3.0.0 software ?

Or does the software automatically detect the STEVAL-C34KAT2 board ?

Does anything need to be added to the device_config.json file ?

I have read the user manual for the STEVAL-C34KAT2, it explains how to connect the board but there's no explanation on how to use it in terms of software.  

Is it just plug and play or are there extra steps required ?

 

 

This topic has been closed for replies.
SimonePradolini
SimonePradoliniBest answer
ST Technical Moderator
Feb 17, 2025 3:25 PM UTC

Hello @johngj 

STEVAL-C34KAT2 is automatically detected and supported by DATALOG2 firmware for STEVAL-STWINBX1.

Simply plug the expansion board to the STWVAL-STWINBX1, power up the board (by plugging USB or using battery) and start the logging (via SD card or USB using the Python-based SDK).

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

1 reply

SimonePradolini
SimonePradoliniBest answer
ST Technical Moderator
Feb 17, 2025 3:25 PM UTC

Hello @johngj 

STEVAL-C34KAT2 is automatically detected and supported by DATALOG2 firmware for STEVAL-STWINBX1.

Simply plug the expansion board to the STWVAL-STWINBX1, power up the board (by plugging USB or using battery) and start the logging (via SD card or USB using the Python-based SDK).

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.