Skip to main content
Associate II
Jul 23, 2024 2:22 PM UTC
Solved

How to manually flash the chip after Model zoo has generated the C-code

Hello! I recently used stm model zoo and deployed an image classification model on a chip. The flashing part is made automatically if the chip is connected, but I was wondering how to do it manually (using another software)?

I get these folders after processing the deployment code but I do not really understand which files to use. 

TECO_0-1721743925812.png

If someone familiar with Model zoo can help me figure this out!

Thanks in advance!

This topic has been closed for replies.
fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Jul 26, 2024 9:49 AM UTC

You want to look at .elf or .bin files and flash those files using STM32CubeProgrammer.

The other option is to open the project in your favorite IDE that supports this STM32 and flash/start the program using the IDE (STM32CubeIDE for example)

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

2 replies

fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Jul 26, 2024 9:49 AM UTC

You want to look at .elf or .bin files and flash those files using STM32CubeProgrammer.

The other option is to open the project in your favorite IDE that supports this STM32 and flash/start the program using the IDE (STM32CubeIDE for example)

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TECOAuthor
Associate II
Aug 2, 2024 10:42 AM UTC

Thank you for your answer Daniel!