Skip to main content
SRath.2
Visitor II
July 18, 2022
Question

How can I import a pre-trained .tflite model into a STM32F413ZH Nucleo board with special operations enabled?

  • July 18, 2022
  • 0 replies
  • 1398 views

Hello Community,

I am trying to integrate a deep neural network into the micro-controller with the help of STM32 Cube IDE. When I try to analyze the model I get the following errors attached as a screenshot. I have to enable the special operations while converting the model to the .tflite model. How can I integrate the model with special operations enabled and analyze it without errors?

Best Wishes,

Siddhesh

This topic has been closed for replies.