Skip to main content
JJone.4
Visitor II
September 28, 2022
Question

How can I configure the STM32 IDE to analyze my tflite file?

I'm using the STM32 IDE, making a project for my Nucleo-G474RE. I've loaded the X-Cube AI software but when trying to analyze my model, it just refuses. I don't get any errors, it goes to about 16% then immediately to 100 and says anaylsis failed. I can run the analysis on STMCubeMX just fine but it won't run on STM32CubeIDE... Is there a setting I'm not seeing or can I transfer the project from cubeMX to IDE so I can write my code?

 [AI:network_1664382959327] C:/Users/veteran/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/windows/stm32ai analyze --name network_1664382959327 -m C:/Users/veteran/Downloads/sine_model.tflite --type tflite --compression none --verbosity 1 --workspace C:\Users\veteran\AppData\Local\Temp\mxAI_workspace6205587743940016258273181889693732 --output C:\Users\veteran\.stm32cubemx\network_output --allocate-inputs --allocate-outputs 

 [AI:network_1664382959327] Getting Flash and Ram size used by the library

 [AI:network_1664382959327] Analyze fail on the AI model

This topic has been closed for replies.