Skip to main content
DLim.16
Associate III
January 6, 2022
Question

Help troubleshooting NanoedgeAI "NEAI_BOARD_ERROR" with STWINKT1B Eval Board

Hi,

I have selected the right target board in NanoedgeAI studio and compiled the library and header files to be included in the STM32CubeIDE project. I am also using the right board: STWINKT1B. Project builds and debugs successfully, but every call from the Nanoedge API returns "NEAI_BOARD_ERROR". For example, this error was observed when calling "neai_anomalydetection_init", "neai_anomalydetection_learn", and "neai_anomalydetection_detect".

Any idea how I can troubleshoot this?

Thanks.

This topic has been closed for replies.

1 reply

Mihir Trivedi
Visitor II
April 11, 2022

Facing the same issue while using ​STM32F411RE, STM32L432KC. Any update on this post ?