Skip to main content
CPutt.1
Associate II
April 15, 2020
Question

FP-AI Sensing in STEVAL-STLKT01V1 Enable UART printf is not working.

Hello,

I am trying using FP-AI Sensing on STEVAL-STLKT01V1 sensortile board. I enabled UART as per the instruction by enabling SENSING1_USE_PRINTF in SENSING1_config.h and SENSING1_USE_PWR_MGNT to 0. I also did 10ms delay for initialization process. But I donot recieve anything in the console after everthing followed as per the instruction. Should there be any changes to be made?

This topic has been closed for replies.

11 replies

NOza.1
Associate
April 20, 2020

Hello,

I am facing the same issue. I am using a STEVAL-STLKT01V1 SensorTile Kit. Please find below steps for reference.

  1. I am using "en.fp-ai-sensing1.zip" SDK and "STM32L476RG-SensorTile" firmware.
  2. Set "SENSING1_USE_PRINTF" as '1' and "SENSING1_USE_PWR_MGNT" set as '0' in SENSING1_config.h file.
  3. Compiled source code in STMCube IDE (Tried on both v1.0.2 and v1.3.0) and generated a SENSING1.bin file.
  4. Flashed boot-loader and application firmware with CleanSENSING1.bat utility.
  5. I found STMicroelectronics Virtual COM Port in TeraTerm. I set 115200 baud-rate, 8N1 mode, and 1 msec transmission delay.
  6. But I could not found any messages in serial port.

Please let me know if I have missed anything.

Thanks

CPutt.1
CPutt.1Author
Associate II
April 20, 2020

Hello Noza,

I followed same steps, I am also facing the same issue. It is not working for me as well, no messages from serial port.

CPutt.1
CPutt.1Author
Associate II
April 20, 2020

Hello Noza,

I dont have the sensor with me right now. Did you try disabling the firewall?

NOza.1
Associate
April 20, 2020

Hi CPutt,

I don't have device in my hand. But I can access via remotely. Will you please help me how can I disable firewall and how it can be helpful to print log on serial console?

CPutt.1
CPutt.1Author
Associate II
April 20, 2020

Hi Noza,

I am not sure if it will be helpful. To disable firewall goto control panel->System and Securtiy->WIndows Defender Firewall and click windows defender firewall on or off and disable windows defender firewall if you have windows 10.

NOza.1
Associate
April 20, 2020

Hi CPutt,

I have found strange thing. The "FP-SNS-ALLMEMS1" SDK successfully compiled and I am able to see logs on UART communication port. It means, hardware successfully working but there is an issue with "FP-AI-SENSING1" SDK.

CPutt.1
CPutt.1Author
Associate II
April 21, 2020

Hi Noza,

Yes, "FP-SNS-ALLMEMS1" works for me as well, couldn't find the issue with "FP-AI-SENSING1" SDK.

NOza.1
Associate
April 21, 2020

Hi CPutt,

Now, It is working for me. We need to virtually link "console.c" file in our project workbench and make below changes in console.c.

int __io_putchar(int ch) {
 while (CDC_Itf_Transmit((uint8_t *)&ch, 1) != USBD_OK);
 /* Transmit zero-length packet to complete transfer */
 while (CDC_Itf_Transmit((uint8_t *)&ch, 0) != USBD_OK);
 return ch;
}
 
int __io_getchar(void) {
 return 1;
}

Please let me know if you still facing any issue.

CPutt.1
CPutt.1Author
Associate II
April 21, 2020

Hi NoZa,

Thank you very much will try this and let you know.

CPutt.1
CPutt.1Author
Associate II
April 21, 2020

Hi NoZa,

Should we create a Newfile with the name console.c and add to the project?