Skip to main content
Associate
Jul 4, 2024 7:50 AM UTC
Question

FP-AI-FACERC Code

Hello, im trying the examples from Fp-ai-facerec but it only have binaries files, so i could'nt understant how it work to config. PLease if anyone have code of this packs please dm me, thanks a lot :3

This topic has been closed for replies.

1 reply

VRICH.1
ST Employee
Aug 1, 2024 2:24 PM UTC

Hello LeHaiAnh,

The FP-AI-FACEREC1 is a demonstration package for evaluation purpose only according to its license terms. The aim is to assess the feasibility of a face recognition application on STM32H7 series. It is delivered in binary file format.

To go further, in the last revision (FP-AI-FACEREC1_v1.3.0) we offer the possibility to see the application code and models used. But STM32_FaceReco AI model is provided without NN parameters. User has to use the provided training scripts to train a model and use X-CUBE-AI to generate the network_data_params.c content. Without properly trained NN parameters, the face recognition function will be ineffective and nonfunctional.

Please contact edge.ai@st.com to get your access.

For production grade quality algorithms, ST is working with Biometrics Partners who are experts in this field.

For contacting ST Biometrics partners please write an email to edge.ai@st.com

Best regards,