Skip to main content
Associate III
Apr 28, 2025 1:20 PM UTC
Solved

Failed to validate a model on N6 target (using both CLI and CubeMX GUI)

Hello, me again.

So I tried to validate a file through cubeAI and ST Edge AI. But always stops by a build problem.

Here is what I do with the CLI:

I followed the Getting started - How to evaluate a model on STM32N6 board .

First I generated the things inside the right file. Its done without any problem.

Einstein_rookie_version_0-1745845942524.png

Einstein_rookie_version_1-1745845964172.png

Then, Because I am using the Nucleo board, I used this command.

python C:\Appl\ST\STEdgeAI\2.0\scripts\N6_scripts\n6_loader.py --n6-loader-config C:\Appl\ST\STEdgeAI\2.0\scripts\N6_scripts\config_n6l.json

(I tried to use the normal one without --n6-loader-config but not working, also build error, so I tried this one)

 

And my json scripts are like this:

Einstein_rookie_version_2-1745846036515.png

Einstein_rookie_version_3-1745846132906.png

However the out come is not right, build error:

Einstein_rookie_version_4-1745846186259.png

And it gives out a comic outcome: I dont know why it have such a error worning.

Einstein_rookie_version_5-1745846222887.png

By the GUI from CubeMX, the log is almost the same.

So I have no idea why, the only reason I can think of is that I dont have a Nucleo board validation program:

Einstein_rookie_version_6-1745846306833.png

As you can see here, it only have a DK board project, and the external Flash might and some other configurations might be different.

So could you help me check what is wrong? thanks a lot in advance.

And by the way if there is really a Nucleo Board validation project, could you please tell me where to find it?

This topic has been closed for replies.
Julian E.
Julian E.Best answer
ST Technical Moderator
Apr 29, 2025 2:43 PM UTC

Hello @Einstein_rookie_version,

 

As of today, it is supported only using IAR, not gcc for the Nucleo board.

We are working on it to make it also compatible with gcc

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Julian E.
Julian E.Best answer
ST Technical Moderator
Apr 29, 2025 2:43 PM UTC

Hello @Einstein_rookie_version,

 

As of today, it is supported only using IAR, not gcc for the Nucleo board.

We are working on it to make it also compatible with gcc

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.