Skip to main content
DAlia.1551
Visitor II
November 24, 2019
Question

Error when loading a model in Cube.AI

I am using CubeAI to load a model from Target Selection. However this model was trained using google Colab. So when I load it and Analyze it I got the error: Unknown Initializer GlorotUniform .

Searching through the web the solution provided is not when building the model but when losing the model but since I don't know how to modify how CubeAI loads the model I am asking for some help here

    This topic has been closed for replies.

    5 replies

    ST Employee
    November 25, 2019

    ​Hi,

    What is the version of the X-CUBE-AI which is used?

    "GlorotUniform" indicates that tf.keras has been used to generate/train the model.

    With X-CUBE-AI 4.1, there is a detection to know if the h5 file ("Keras" model) has been create with tf.keras or keras.

    If you use X-CUBE-AI 4.1, can you try with the command line tools to import the h5 file:

    > set TF_KERAS=1

    > stm32ai analyze -m <tf-keras-model-path>

    br,

    Jean-Michel

    David Wallén
    Associate III
    June 4, 2020

    Hi Jean-Michel,

    I faced the same issue as DAlia.1551 described. I build and trained my model in Google Colab using Tensorflow version 2.2.0 which embeds Keras version 2.3.0.

    Using the command you provided (thanks for that btw) gave me the insight that X-CUBE-AI (I have version 5.0.0) only supports Keras 2.2.4-tf, as described in this error message:

    Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0)
    -- Importing model
    Using TensorFlow backend.
    INVALID MODEL: Couldn't load Keras model /Users/David/Downloads/model.h5, error: Model saved with Keras 2.3.0-tf but <= 2.2.4-tf is supported

    My question now if you have the intention to in the near future support these newer versions of Tensorflow (and Keras)? When can this be expected?

    If the expected support from your side is far away (months away) what work-around do you suggest for me? Rebuild the whole model using an earlier version of Keras?

    Thanks in advance!

    Best Regards,

    David

    ST Employee
    June 4, 2020

    Hi David,

    This issue has been identified and we work on it for the future release (date not yet committed). I will complete my answer when a date is committed.

    • Currently a possible work-around is to convert the h5 file to a tflite file with the TF Lite converter BUT this is not guarantee. TFLite file format is more portable but sometime there is also some modifications which are not always covered by the X-CUBE-AI TF Lite importer. And all Keras layers are not necessarily convertible through the TF Lite operators.
    converter = tf.compat.v1.lite.TFLiteConverter.from_keras_model_file(<keras_model_path>)
    tfl_model = converter.convert()
    open(tfl_file_path, "wb").write(tfl_model)

    • Other work-around, through Google Colab is to use a TensorFlow version 1.x. if compatble with your script
    %tensorflow_version 1.x

    https://colab.research.google.com/notebooks/tensorflow_version.ipynb#scrollTo=aR_btJrKGdw7

    br,

    Jean-Michel

    David Wallén
    Associate III
    June 4, 2020

    Hi Jean-Michel,

    Many thanks for your prompt reply, very impressive!

    To use a TF Lite format was actually my first approach, but there I faced an even more ambiguous error. simply "INTERNAL ERROR".

    I tried it again now using

     tf.compat.v1.lite.TFLiteConverter.from_keras_model_file()

    as you are suggesting instead of

    tf.lite.TFLiteConverter.from_keras_model()

    which I used before. But I still get "INTERNAL ERROR" in CubeMX AI plugin.

    Using the cli version of stm32ai as you suggested does not lead to a lot of extra information, as you can see here:

    David@Davids-MacBook-Air-3:~/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac$ ./stm32ai analyze -m ~/Downloads/dnn_multivar_multistep_classifier_targetsteps_1_L1_8_L2_8_sigmoid_model_nepochs_10_nstepsperepoch_100_date_20-06-04.h5.tflite 
    Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0)
    -- Importing model
    INTERNAL ERROR: 
     
    Creating report file /Users/David/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac/stm32ai_output/network_analyze_report.txt
     
    INTERNAL ERROR: 

    and the crash report file does not contain any information that is useful (at least not to my eye), but perhaps you can make something of it:

    David@Davids-MacBook-Air-3:~/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac$ cat /Users/David/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac/stm32ai_output/network_analyze_report.txt
    Neural Network Tools for STM32 v1.2.0 (AI tools v5.0.0)
    Created date : 2020-06-04 16:02:10
     
    Exec/report summary (analyze err=-1)
    ------------------------------------------------------------------------------------------------------------------------
    error : INTERNAL ERROR: 
    model file : /Users/David/Downloads/dnn_multivar_multistep_classifier_targetsteps_1_L1_8_L2_8_sigmoid_model_nepochs_10_nstepsperepoch_100_date_20-06-04.h5.tflite
    type : tflite (tflite)
    c_name : network
    compression : None
    quantize : None
    L2r error : NOT EVALUATED
    workspace dir : /Users/David/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac/stm32ai_ws
    output dir : /Users/David/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/5.0.0/Utilities/mac/stm32ai_output
     
     
    INTERNAL ERROR: 
     
    Evaluation report (summary)
    --------------------------------------------------
    NOT EVALUATED

    When you mention that I could change to TF version 1.x I would really like to avoid that since I have built up my entire architecture around TF2.0 and I would really not like to go back to 1.x with it's non eager executions and such, I hope you understand.

    Do you think it would work if I rebuilt it using the "pure keras" library (i.e. using "import keras" instead of "import tf.keras"? To be honest the way Keras and TF versions work now after the Keras integration is a bit confusing to me...

    Let me know what you think.

    Thanks in advance!

    Best Regards,

    David

    FSach.1
    Visitor II
    September 22, 2020

    Hi,

    I've faced the same issue as DAlia.1551 and David. I've developed a neural network model using TF 2.x, and then tried importing the .h5 file to my STM32. Suggested solutions to this problem have not work in case of my recurrent neural network, as I couldn't afford downgrading to TF version 1.x, nor did the conversion of the model to TFlite work because of the presence of cells such as LSTM.

    What worked however, was changing one line of code that directly affects how model is exported:

    import keras # Correct
    from tensorflow import keras # Will cause the Unknown Initializer GlorotUniform
     
    model.save("model_name.h5")

    Let me know if it helped anyone.

    Best Regards,

    Filip