Skip to main content
Associate II
May 20, 2024 3:42 PM UTC
Solved

Error in STM32CUBEIDE while analyzing a tensorflow lite model [X CUBE AI]

good morning, I'm trying to import a neural network for NILM (non-intrusive load monitoring) in the stm32 environment, but I can't complete the analysis due to the presence of the error: 

INTERNAL ERROR: unpack_from requires a buffer of at least 122836864 bytes for unpacking 4 bytes at offset 122836860 (actual buffer size is 1654784)

 The network is CNN type and I'm working with xcube ai v. 9.0.0 and stm32cubeide 1.15.1

I'm asking anyone if they know how I can solve the problem of the buffer size.

Belolw I share the link for the TFlite model (seq2point_CNN_converted_model.tflite), thanks in advantace.

https://drive.google.com/file/d/1FhDdYCNd0y86SptZ5FHCSjpUQdkdxXZ9/view?usp=drive_link

This topic has been closed for replies.
fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Jul 17, 2024 3:50 PM UTC

Seems that your model is malformed I can't even open it with Netron.

At this point the tool is still using tensorflow 2.15.1, maybe the error comes from a more recent version of tensorflow

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

fauvarque.daniel
fauvarque.danielBest answer
ST Employee
Jul 17, 2024 3:50 PM UTC

Seems that your model is malformed I can't even open it with Netron.

At this point the tool is still using tensorflow 2.15.1, maybe the error comes from a more recent version of tensorflow

 

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.