Skip to main content
Associate
Dec 19, 2024 5:36 PM UTC
Solved

Error analysing LSTM model using X-Cube-AI:INTERNAL ERROR : Unkonwn dimensions : CH

When I analyze the ONNX model in CubeAl,it says INTERNAL ERROR : Unkonwn dimensions : CH.The code of the model is simple as follows,input_size = 1 hidden_size = 1 output_size = 1 num_layers = 1
I don't know why and I will really appreciate any advice or workarounds. Thank you:

class LSTMNet(nn.Module):
def __init__(self, input_size, hidden_size, output_size, num_layers=1)
super(LSTMNet, self).__init__()
self.lstm = nn.LSTM(input_size, hidden_size, num_layers, batch_first=False) # batch_first=False
self.fc = nn.Linear(hidden_size, output_size)

def forward(self, x):
h0 = torch.zeros(num_layers, x.size(1), hidden_size).to(x.device)
c0 = torch.zeros(num_layers, x.size(1), hidden_size).to(x.device)
out, _ = self.lstm(x, (h0, c0))
out = self.fc(out[-1, :, :])
return out

This topic has been closed for replies.
Julian E.
Julian E.Best answer
ST Technical Moderator
Dec 20, 2024 1:07 PM UTC

Hello @Wangxingkun ,

 

What version of ST Edge AI are you using?

I tried it and I do not get errors...

This is the version I have (the last I believe)

JulianE_0-1734699970619.png

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

8 replies

Associate
Dec 19, 2024 5:48 PM UTC

And this is my complete training code, if you know the reason why please reply me, thank you !!!

class SequenceDataset(Dataset):
def __init__(self, sequences, labels):
self.sequences = sequences
self.labels = labels

def __len__(self:(
return len(self.labels)

def __getitem__(self, idx):
return torch.Tensor(self.sequences[idx]), torch.Tensor(self.labels[idx])

class LSTMNet(nn.Module):
def __init__(self, input_size, hidden_size, output_size, num_layers=1:(
super(LSTMNet, self).__init__()
self.lstm = nn.LSTM(input_size, hidden_size, num_layers, batch_first=False) # batch_first=False
self.fc = nn.Linear(hidden_size, output_size)

def forward(self, x):
h0 = torch.zeros(num_layers, x.size(1), hidden_size).to(x.device)
c0 = torch.zeros(num_layers, x.size(1), hidden_size).to(x.device)
out, _ = self.lstm(x, (h0, c0))
out = self.fc(out[-1, :, :])
return out

input_size = 1
hidden_size = 1
output_size = 1
num_layers = 1
num_epochs = 120
batch_size = 32
learning_rate = 0.001

num_samples = 1000
sequence_length = 15
sequences = torch.rand(num_samples, sequence_length, input_size)
labels = torch.randint(0, 2, (num_samples, 1))

dataset = SequenceDataset(sequences.numpy(), labels.numpy())
train_loader = DataLoader(dataset, batch_size=batch_size, shuffle=True)

model = LSTMNet(input_size, hidden_size, output_size, num_layers)
criterion = nn.BCEWithLogitsLoss()
optimizer = optim.Adam(model.parameters(), lr=learning_rate)

model.train()
for epoch in range(num_epochs):
for seqs, lbls in train_loader:
seqs = seqs.permute(1, 0, 2)
outputs = model(seqs)
loss = criterion(outputs, lbls)
optimizer.zero_grad()
loss.backward()
optimizer.step()
print(f'Epoch [{epoch+1}/{num_epochs}], Loss: {loss.item():.4f}')

example_input = torch.rand(sequence_length, 1, input_size)
torch.onnx.export(model, example_input, 'lstm_model.onnx',
input_names=['input'],
output_names=['output'],
dynamic_axes={'input': {1: 'batch_size', 0: 'sequence_length'},
'output': {0: 'batch_size'}})
print('Model exported as lstm_model.onnx')
Julian E.
ST Technical Moderator
Dec 20, 2024 9:24 AM UTC

Hello @Wangxingkun,

 

I am not an expert regarding pytorch so I will need my colleagues for a more complete answer. But they are in vacation. In the meantime, you can take a look at this code that works and should help you

 

import torch
import torch.nn as nn

class LSTM(nn.Module):
 def __init__(self, input_size, hidden_size, num_layers, num_output=1):
 super(LSTM, self).__init__()
 self.num_layers = num_layers
 self.input_size = input_size
 self.hidden_size = hidden_size
 self.num_output = num_output

 self.lstm = nn.LSTM(input_size=input_size, hidden_size=hidden_size,
 num_layers=num_layers, batch_first=False)

 self.fc = nn.Linear(hidden_size, num_output)

 def forward(self, x, device='cuda'):

 ula, (h_out, _) = self.lstm(x) 
 out = self.fc(h_out[-1]) 
 return out

# If not 1 : error
# other we can put anything
input_size = 10
hidden_size = 10
num_layers = 1
num_output = 10

model = LSTM(input_size, hidden_size, num_layers, num_output)

model.eval()

dummy_input = torch.randn(1, 128, input_size) # Batch size 1, Sequence length 128, Input size 10

onnx_file_path = "simple_lstml.onnx"
torch.onnx.export(model, dummy_input, onnx_file_path, 
 input_names=['input'], output_names=['output'])

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate
Dec 20, 2024 11:54 AM UTC

Thank you very much Julian, I have tried your code but it still says 'INTERNAL ERROR : Unkonwn dimensions : CH'.It seems that as long as there is an LSTM layer in the model, there will be the following error. If it is a fully connected layer, there will be no such error.But in my project, the LSTM layer is necessary, and I don't know how to fix it.It makes me a little frustrated.